2024-07-30 8:01 AM
Some parts of my application are driven by the SysTick timer, and I got into the practice of adding `HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI)` while polling a flag, knowing that the SysTick interrupt will wake the microcontroller and update the flag as needed.
This got me thinking, can I do the same in the `HAL_Delay` function? The implementation of `HAL_Delay` is this:
__weak void HAL_Delay(uint32_t Delay)
{
uint32_t tickstart = HAL_GetTick();
uint32_t wait = Delay;
/* Add a freq to guarantee minimum wait */
if (wait < HAL_MAX_DELAY)
{
wait += (uint32_t)(uwTickFreq);
}
while((HAL_GetTick() - tickstart) < wait)
{
}
}
Can I change it to this:
__weak void HAL_Delay(uint32_t Delay)
{
uint32_t tickstart = HAL_GetTick();
uint32_t wait = Delay;
/* Add a freq to guarantee minimum wait */
if (wait < HAL_MAX_DELAY)
{
wait += (uint32_t)(uwTickFreq);
}
while((HAL_GetTick() - tickstart) < wait)
{
HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);
}
}
with no problem? I need to be aware of something? Is there any reason why the HAL does not do it by default?
Looking at the datasheet of the microcontroller I am using (STM32F405), the wakeup time in this situation is typically 13 us, which I think is not that bad (correct me if I am wrong).
I would even use the sleep mode (which has a typical wakeup time of 5 cycles, or ~24ns at 168MHz), but `HAL_PWR_EnterSLEEPMode`'s doc-comment states that the SysTick is stopped (although the source code of the function doesn't appear to stop the SysTick, but I am not sure I can rely on that).
2024-08-04 4:20 AM
Dear @RodrigoMoraes ,
What is the clock source of your function using Systick interrupt ? I know it is a basic question but I’am asking because systick is off while device is in STOP mode and can not wake your system each 13us . You have most probably something else doing that such as RTC interrupt or simply your system is not entering STOP mode . Can you remove the debugger and keep the Application in standalone within ST-Link . Let us know .
STOne-32
2024-08-05 7:40 AM
Sorry, you are right, STOP mode does indeed stop the Systick. I am actually using `HAL_PWR_EnterSLEEPMode`, but while reading its documentation (the "doc-comment states that the SysTick is stopped") and reading this article, I confused the two. I revised the previous project where I originally used the pattern mentioned (a stm32c031), and I use `HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);` while busy waiting on a flag.
So, going back to my intended question, is there any problem adding `HAL_PWR_EnterSLEEPMode` inside `HAL_Delay`?
And looking at the doc-comment in my previous project, it does not have the note about systick being stopped, maybe the project I am currently working on have a error due to being generated in a older version of STM32CubeIDE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.