2015-04-07 9:27 AM
Hi,
I am trying to run a simple program on my new Nucleo board,
I made this program in order to turn on and off the green led when i press the user's button (the blue one),
#include ''stm32f4xx.h''
#include ''stm32f4xx_nucleo.h''
#include ''system_stm32f4xx.h''
#include ''stm32f4xx_hal_gpio.h''
#include ''stm32f4xx_hal_rcc.h''
GPIO_InitTypeDef GPIO_InitStructure;
int
main(
void
) {
HAL_Init();
__GPIOA_CLK_ENABLE();
GPIO_InitStructure.Pin = GPIO_PIN_5;
GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStructure.Pull = GPIO_PULLUP;
GPIO_InitStructure.Speed = GPIO_SPEED_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
__GPIOC_CLK_ENABLE();
GPIO_InitStructure.Pin = GPIO_PIN_13;
GPIO_InitStructure.Mode = GPIO_MODE_INPUT;
GPIO_InitStructure.Pull = GPIO_PULLDOWN;
GPIO_InitStructure.Speed = GPIO_SPEED_FAST;
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
while
(1) {
if
(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)) {
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
}
else
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
}
}
But i am getting wrong result:
- when i press the user's button, nothing happen,
- when i keep pressing the user's button and i restart (by pressing the black button), i get good result,
It seems like the program checks the state of the blue button only at the first run, i don't know why,
Please help me if you have any ideas of what the problem comes from, or if you have a running program that switch the led on button press.
Thank you,
#stm32f401re
2015-04-07 10:19 PM
Hi samy,
do you have system clock configuration in your program?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.