2015-04-07 9:22 AM
Hello,
I am trying to run a simple program on my new Nucleo board, I made this program in order to turn on and off the green led when i press the user's button (the blue one), http://pastebin.com/9Q7KxsVA &sharpinclude ''stm32f4xx.h'' &sharpinclude ''stm32f4xx_nucleo.h'' &sharpinclude ''system_stm32f4xx.h'' &sharpinclude ''stm32f4xx_hal_gpio.h'' &sharpinclude ''stm32f4xx_hal_rcc.h'' GPIO_InitTypeDef GPIO_InitStructure; int main(void) { HAL_Init(); __GPIOA_CLK_ENABLE(); GPIO_InitStructure.Pin = GPIO_PIN_5; GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Pull = GPIO_PULLUP; GPIO_InitStructure.Speed = GPIO_SPEED_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStructure); __GPIOC_CLK_ENABLE(); GPIO_InitStructure.Pin = GPIO_PIN_13; GPIO_InitStructure.Mode = GPIO_MODE_INPUT; GPIO_InitStructure.Pull = GPIO_PULLDOWN; GPIO_InitStructure.Speed = GPIO_SPEED_FAST; HAL_GPIO_Init(GPIOC, &GPIO_InitStructure); while (1) { if (HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET); } else { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET); } } } But i am getting wrong result: - when i press the user's button, nothing happen, - when i keep pressing the user's button and i restart (by pressing the black button), i get good result, It seems like the program checks the state of the blue button only at the first run, i don't know why, Please help me if you have any ideas of what the problem comes from, or if you have a running program that switch the led on button press. Thank you, #stm32-st-nucleo-f401re2015-04-07 10:17 PM
Hi samy,
do you have system clock configuration in your program?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.