cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4 weird crashing

EPora.1
Associate II

Hi everyone,

I'm dealing with some difficult problem for quite a while. I am using an stm32f411ce running on 80mhz. I have a code in which I am reading data from some sensors and then processing it. when I run the code it crashes randomly with different error calls. the processing code itself is proven to not be the problem, I have tested it on my pc with VScode. Here is my main setup and I2C setup. Thus this is the only code other then the processing it must be the problem.

The clock and simple pinout setup:

// set the HSEON bit high
	RCC ->CR |= RCC_CR_HSEON;
	//wait for the HSE to be ready
	while (!(RCC ->CR & (1<<17)));
	//while (!(RCC->CR & (1<<17)));
	
	//set up the power registers
	RCC ->APB1ENR |= RCC_APB1ENR_PWREN;
	RCC ->AHB1ENR |= RCC_AHB1ENR_GPIOBEN;
	PWR->CR |= (3<<14); 
	FLASH->ACR = (1<<8) | (1<<9)| (1<<10)| (2<<0);
	uint32_t temp = FLASH ->ACR; //it is recommended to read the register
	//FLASH->ACR = (1<<8) | (1<<9)| (1<<10);
	
	RCC->AHB1ENR |= (1 << 1);
	
	GPIOB ->MODER |= GPIO_MODER_MODE2_0; //Generel prupose output mode
	GPIOB ->MODER &= ~GPIO_MODER_MODE2_1;
	
	GPIOB ->MODER |= GPIO_MODER_MODE13_0; //Generel prupose output mode 
	GPIOB ->MODER &= ~GPIO_MODER_MODE13_1;
	
	GPIOB ->MODER |= GPIO_MODER_MODE14_0; //Generel prupose output mode
	GPIOB ->MODER &= ~GPIO_MODER_MODE14_1;
	
	GPIOB ->MODER |= GPIO_MODER_MODE15_0; //Generel prupose output mode
	GPIOB ->MODER &= ~GPIO_MODER_MODE15_1;
	
 
	
	
	//OTYPER:
	//0: Output push_pull (reset state)
	//1: Output open-drain
	GPIOB ->OTYPER &= ~(GPIO_OTYPER_OT_2); //push_pull
	GPIOB ->OTYPER &= ~(GPIO_OTYPER_OT_13); //push_pull
	GPIOB ->OTYPER &= ~(GPIO_OTYPER_OT_14); //push_pull
	GPIOB ->OTYPER &= ~(GPIO_OTYPER_OT_15); //push_pull
	
	
	//OSPEEDR:
	//x0: Low speed
	//01: Medium speed
	//11: High speed
	GPIOB ->OSPEEDR |= (3 << 4);
	GPIOB ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR13;
	GPIOB ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR14;
	GPIOB ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR15;
	
	
	//PUPDR:
	//00: No pull-up, pull-down
	//01: Pull-up
	//10: Pull-down
	//11: Reserved
	GPIOB ->PUPDR &= ~(GPIO_PUPDR_PUPD2); //No pull-up, pull-down
	GPIOB ->PUPDR &= ~(GPIO_PUPDR_PUPD13); //No pull-up, pull-down
	GPIOB ->PUPDR &= ~(GPIO_PUPDR_PUPD14); //No pull-up, pull-down
	GPIOB ->PUPDR &= ~(GPIO_PUPDR_PUPD15); //No pull-up, pull-down
 
	//set the pll scalers
	RCC ->PLLCFGR &= ~(63 << 0); // PLLM div4
	RCC ->PLLCFGR |= 4;
	
	RCC ->PLLCFGR &= ~(511 << 6);
	RCC ->PLLCFGR |= (80 << 6); //PLLN scale80
	
	RCC ->PLLCFGR &= ~(3 << 16); //PLLP div2
	//RCC ->PLLCFGR &= ~RCC_PLLCFGR_PLLP;
	
	RCC ->PLLCFGR |= (6 << 24); //PLLQ div3
 
	//setting post-pll prescalers
	RCC ->CFGR |= (4 << 10); //PPRE1/APB1 div2
	
	RCC ->CFGR &= ~(7 << 13); //PPRE2/APB2 div1
	
	RCC ->CFGR &= ~(1 << 7); //HPRE/AHB div1
 
	//tell the PLL to use the HSE
	RCC ->PLLCFGR |= (1 << 22);
	
	//setting the main pll on
	RCC ->CR |= (1 << 24);
	//wait for the PLL to be ready
	while (!(RCC ->CR & RCC_CR_PLLRDY));
	//while (!(RCC->CR & (1<<25)));
 
	//set the system clock input to PLL RCC_CFGR -> SW
	RCC ->CFGR |= (1 << 1);
	//wait for the system clock sorce to be set to PLL
	while (!(RCC ->CFGR & (1 << 3)));
	
	SystemCoreClockUpdate();

The I2C setup code:

//enable the I2C perefiral
	RCC->AHB1ENR |= (1<<1);  // Enable GPIOB CLOCK
	RCC ->APB1ENR |= RCC_APB1ENR_I2C1EN; //enable the I2C1
 
	
	
	
	//MODER:
	//00: Input mode
	//01: Generel prupose output mode
	//10: Alternate function mode
	//11: Analog mode
	GPIOB ->MODER &= ~GPIO_MODER_MODE8_0; //Alternate function mode
	GPIOB ->MODER |= GPIO_MODER_MODE8_1;
	GPIOB ->MODER &= ~GPIO_MODER_MODE9_0; //Alternate function mode
	GPIOB ->MODER |= GPIO_MODER_MODE9_1;
	
	//OTYPER:
	//0: Output push_pull (reset state)
	//1: Output open-drain
	GPIOB ->OTYPER |= GPIO_OTYPER_OT8; //open-drain
	GPIOB ->OTYPER |= GPIO_OTYPER_OT9; //open-drain
	
	//OSPEEDR:
	//x0: Low speed
	//01: Medium speed
	//11: High speed
	GPIOB ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR8; //High speed
	GPIOB ->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR9; //High speed
	
	//PUPDR:
	//00: No pull-up, pull-down
	//01: Pull-up
	//10: Pull-down
	//11: Reserved
	GPIOB ->PUPDR &= ~GPIO_PUPDR_PUPD8;
	GPIOB ->PUPDR &= ~GPIO_PUPDR_PUPD9;	
	//GPIOB ->PUPDR |= (1 << 16) | (1 << 18);
 
	
	//enable pins 8 and 9 I2C alternate function
	GPIOB ->AFR[1] |= (1 << 2) | (1 << 6);	//set pins PB8 and PB9 to I2C alternate-function
	
	
	
	//reset the I2C
	I2C1 ->CR1 |= (1<<15);
	I2C1 ->CR1 &= ~(1<<15);
	
	
	//set the I2C CR2 input clock frequency
	I2C1 ->CR2 |= (40 << 0); //40 is the APB1 clock, make sure thats it is set up correctly
	
	
	//CRR register
	//      Tr(scl) + Tw(sclh)
	//CRR = -------------------
	//            Tpclk1
	//Tr(scl) = 300ns
	//Tw(sclh) = 600ns
	//Tpclk1 = (1 / 40)ns = 25ns //1 over the PCLK1 frequency
	//CCR = 4
	I2C1 ->CCR |= (4<<0);
	
	//TRISE register
	//         Tr(scl)
	//TRISE = ---------- + 1
	//         Tpclk1
	//Tr(scl) = 300ns
	//Tpclk1 = (1 / 40)ns = 25ns //1 over the PCLK1 frequency
	//TRISE = 12 + 1
	I2C1 ->TRISE |= (13<<0);
	
	
	/*
	//select the I2C mode: 0 for standard and 1 for fast
	I2C1 ->CCR &= ~(1 << 15);
	
	//select the I2C CCR duty bit
	I2C1 ->CCR &= ~(1 << 14); //same as the I2C mode
	*/
	
	//select the I2C mode: 0 for standard and 1 for fast
	I2C1 ->CCR |= (1 << 15);
	
	//select the I2C CCR duty bit
	I2C1 ->CCR |= (1 << 14); //same as the I2C mode
	
	//I2C perefiral enable
	I2C1 ->CR1 |= (1 << 0);

I would love to have some help thanks!

Eyal

Edit:

here is the timer setup too

	RCC ->APB2ENR |= (1 << 16); //enable the TIM9 clock
	//timers clock is 86mhz
	//TIM9 ->PSC |= 10000-1; //clock fraquency -1 to get a 10khz pulse
	//TIM9 ->PSC |= 12500-1; //clock fraquency -1 to get a 10khz pulse
	TIM9 ->PSC |= 8000-1; //clock fraquency -1 to get a 10khz pulse
	TIM9 ->ARR |= 0xFFFF; //set the maximum value to be the max possible
	
	TIM9 ->CR1 |= (1 << 0); //enable the timer
	
	while (!(TIM9 ->SR & (1 << 0))); //wait for the timer ready bit to set 

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User

Is this a "known good" board like Nucleo/Disco? If not, you should try your code on one of those.

Looks good at the first sight. Try reading out and checking the RCC registers content. Try doing something simpler, like a blinky, check if it is rock stable. Check power supply. Check all VDD and VSS connections, including the analog. I am talking about bad solder joints. Check that voltage on VCAP is as expected and rock stable. Check VCAP connections.

JW

Thanks for your response! I'll check it all out.

I'm using a custom board.

Eyal

Hi again, I've checked all of the connections and they look good. the VCAP voltage is around 1.3V and stable, is this ok? also, the VCAP pin is connected to ground through a 4.7nF cap, is this ok?

Thanks, Eyal

EPora.1
Associate II

Problem Solved!

I have noticed that I put a 4.7nF cap instead of a 4.7uF cap on the Vcap pin

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.