2021-08-06 1:33 AM
Hello
Our new product use a STM32F427 and a ADC(AD7768-4) the data input connection is the SAI(serial audio interface). The STM32F4 SAI mode is the slave mode.
The ADC sends SAI_SD signal and SAI_FS at rising edge.
Therefore, we think that the STM32F4 clock strobing is the falling edge.
Is our understanding of this correct?
Does the STM32F4 clock strobing edge mean the SAI_SD signal and SAI_FS latching point?
2021-08-06 2:43 AM
Which edge of SAI_SCK is used to strobe (yes, latch) data, can be selected in SAI_xCR1.CKSTR.
JW
2021-08-06 7:45 AM
Dear waclawek.jan san
Thank you for your reply.
We understood the strobe and SAI_SCK is used to strobe data only.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.