2012-04-15 5:51 AM
I am using the STM32F4 discovery board to generate a PWM signal using TIMER 1, channel 1, and am using GPIO A8 in AF mode. When i run the code there is no pulse generated, but the pin A8 gets pulled up to Vcc.
The above mentioned happens for TIMER 8 too(Channel 1, GPIO PC6). I did not have any problem configuring the other Timer's. Since i intend to use the repetition counter i have to work with Timer 1 and Timer 8. I would really appreciate it if someone could help me out here. The code i attached below: #include ''stm32f4_discovery.h'' TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; uint16_t CCR1_Val = 250; uint16_t PrescalerValue = 0; void TIM_Config(void); int main(void) { /* TIM Configuration */ TIM_Config(); PrescalerValue = (uint16_t) ((SystemCoreClock /2) / 28000000) - 1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 665; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM1, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM1, ENABLE); /* TIM 1 enable counter */ TIM_Cmd(TIM1, ENABLE); while (1) {} } void TIM_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; /* TIM1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); /* GPIOA clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* GPIOC Configuration: TIM1 CH1 (PA8) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect TIM1 pins to AF2 */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1); } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ while (1) {} } #endif2012-04-15 6:17 AM
...
/* TIM1 counter enable */ TIM_Cmd(TIM1, ENABLE); /* TIM1 Main Output Enable */ TIM_CtrlPWMOutputs(TIM1, ENABLE); ...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.