STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 I2C init failed

Posted on April 13, 2012 at 19:09ATTENTION! The following code do not work for STM32 I2C while looking good:void I2C_Ini(void){ I2C_InitTypeDef I2C_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; // I2C RCC RCC_APB1PeriphClockCmd(RCC_APB1Periph_...

ivainc by Associate III
  • 2922 Views
  • 6 replies
  • 0 kudos

Check if a uC is alive or dead

Posted on April 11, 2012 at 18:39I wonder if someone could help me. I recently have developed my own PCB board. I've soldered all the components, and now I want to starting downloading some firmware to the uC (STM32F407ZG - LQFP144pin). For my surpr...

tecnico23 by Associate II
  • 9446 Views
  • 28 replies
  • 0 kudos

Doc error TRM STM32F4: PC13..15 only ONE output?

Posted on April 16, 2012 at 09:07In TRM STM32F4 (RM0090) it says in Chapter 4 ''PWR'', 4.1.2 ''Battery...'': Note ''Due to the fact that the switch only sinks a limited amount of current (3 mA), the use of GPIOs PC13 to PC15 are restricted: only one...

flyer31 by Senior
  • 705 Views
  • 0 replies
  • 0 kudos

STM32F4 PWM genertation using TIM1 and TIM8

Posted on April 15, 2012 at 14:51I am using the STM32F4 discovery board to generate a PWM signal using TIMER 1, channel 1, and am using GPIO A8 in AF mode. When i run the code there is no pulse generated, but the pin A8 gets pulled up to Vcc.  The a...

anoop by Associate II
  • 1715 Views
  • 1 replies
  • 0 kudos

SD Bootloader Interrupt Problem

Posted on April 12, 2012 at 17:18Hi,I have written a Bootloader that looks at the micro sd card and loads firmware.bin file into address 0x00800C000 and jumps program execution to 0x00800C004. I have changed the Flash address in the code that is loa...

ADC Sample Time Selection

Posted on April 10, 2012 at 22:18While it is clear how to configure the ADC sample time, the documentation doesn't provide insight into why one might prefer 239.5 cycles over 13.5 cycles, or the impact of selecting 7.5 cycles (I'm guessing 6 bits of...

uClinux_on_stm32.patch.gz

Posted on January 03, 2012 at 07:14Hello. I'm trying to run ucLinux on STM32. I'm looking for uClinux_on_stm32.patch.gz that is mentioned in the Application note AN3012 (Getting started with uClinux). Where can I find this patch? Thanks in advance, ...

STM32F4-Discovery + LCD

Posted on March 16, 2012 at 16:53Hello everyone, I'm trying to add an LCD to my stm32f4-discovery using FSMC driver/protocol and I'd like to know how can I do. I have seen STEVAL-CCM002V1 but seems working only with STM32F10xxx. Is there an easy so...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.