2017-11-04 12:19 AM
Hi:
Can STM32F401's PCM be set as the following formats ?
PCM Slave , FS=8Khz ,BITS=16, Mono ( which means BCLK= 8khz * 16 = 128Khz)
After some tests , i find the PCM can only be used as stereo mode (BCLK = 8khz * 16 *2), is that true?
Thanks !!!
#stm32f4 #i2s #pcm2017-11-04 12:36 AM
When both PCM master device and STM32F401 set with : 8Khz,16bits,stereo, it works fine.
When using mono mode, it seems that STM32F401 can recieve/send all bits ,but the bit position is mismatched.
Can someone could help me with this?
2017-11-15 12:49 AM
Hello,
Can you provide more details about your application? Are you trying to read data from a digital microphone with an audio sampling frequency= 8KHz?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.