2014-08-12 9:35 AM
Hi,
I have a problem with my steval-ccm008v1 evaluation board. When I load ST Mass Storage example everything is fine. I connect my board to PC and format it through Windows. Then I see a filesystem on my board and I can create some files on it. But after reconnecting (or reseting) the board the filesystem falls and I need to format it every time I connect my board via USB. Thanking in an anticipation, Aveal. #nand-flash-msc #stm32f4 #steval-ccm008v12014-10-08 3:15 AM
Hi
,
Aveal
!
For
solve this problem,
we need
to have
the source code
,
because
demoboard
have
a little
number of people
,
however,
just
a Board with
nand
flash
memory
have many.
If possible
, put
the complete project
for download.
2014-10-08 8:15 AM
NAND with large erase blocks doesn't really lend itself to a simple MSC or FAT File System usage.
2014-10-08 10:05 AM
Strange
, but
all
flash drives
work with
Nand
flash memory
, and
examples
STEVAL_CCM006V1
-
STEVAL_CCM008V2
also
to work with
NAND
flash
.
The use of a
Look
up table
(
LUT)
should help
with recording
sectors.
Yes
and
do not exclude the possibility
of external
memory
(static
RAM
,
SDRAM
for
stm32f42x
),
or
for some
enough
internal memory
.
By the way
,
dear
Clive1
,
you can't tell
where you can find
suorce
code
from
STEVAL_CCM008V1
,
or perhaps
he is
do you
?
2014-10-08 10:22 AM
Yes, but your SD Card or USB Flash present you with a micro processor that handles the large blocks (128KB or whatever) and allows you to read/write 512 byte sectors, multiple sectors, and deals with ALL the dirty details about error correction, deblocking and block mapping/remapping, and wear leveling.
So unless you have a 128KB RAM buffer to play with, or you copy data to a new block on the fly, it's definitely not EASY to deal with raw NAND devices on a micro like the STM32.You'd likely have to speak to your local ST Rep or FAE, and sign appropriate NDA, IP and licencing documents/releases.2014-10-08 10:57 PM
Hello ,
Please tell,which NAND FLASH you are using? For ONFI NAND FLASH ,it supports only upto 1Gb. For making it working -> Please make following change: Replace statement in this function ''void FSMC_NAND_ONFI_Compliance(void)'' if(Buff[6]& 0x10) COPY_STATE = COPY_BACK_SUPPORTED; else COPY_STATE = COPY_BACK_NOT_SUPPORTED; with if(0) COPY_STATE = COPY_BACK_SUPPORTED; else COPY_STATE = COPY_BACK_NOT_SUPPORTED; It will work without CopyBack command. ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.