2015-01-28 2:47 PM
Hello everyone,
I have currently a system which is using ADC1/2 in dual ADC mode regular interleaved with Timer 3 TGRO and DMA. I want to use the ADC3 regular mode with 4 channels.Is the common initialization structure is only used for dual/triple mode or it applies also to the ADC3 in single mode?Can we use them all on regular mode or I need to move ADC1/2 on injected mode and use ADC3 alone in regular mode?The goal is to have ADC1/2 in dual regular interleaved external trigger or dual injected alter trigger and ADC3 4 channels in regular single mode.Thank you #adc #stm32f42015-01-28 5:05 PM
In Dual mode ADC1 and ADC2 are bonded. ADC3 should not be effected and should function autonomously.
2015-01-29 6:34 AM
Based on this commun configuration.
ADC_CommunStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommunStructure.ADC_Mode = ADC_DualMode_Interl;
ADC_CommunStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_2;
ADC_CommunStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_8Cycles;
ADC_CommonInit(&ADC_CommunStructure);
How the DMA will behave for the ADC3? Is it not applying to ADC3 and simply copy the data from ADC3 to memory like inADC_DMAAccessMode_Disabled ?
Thank you!
2015-01-29 7:38 AM
How the DMA will behave for the ADC3? Is it not applying to ADC3 and simply copy the data from ADC3 to memory like in ADC_DMAAccessMode_Disabled ?
I'd expect the ADC3->DR to behave as it always does, and *not* like reading the CDR (Common Data Register) which is what bonded ADC1+ADC2 would be using. How long could it possibly take to try this?
2015-01-29 8:02 AM
Ok thank you.
It will not take long time but unfortunately I am in the process on buying the compiler and right now my evaluation license is expired so might have to wait a few days ...I will post the result once I have it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.