2013-10-02 8:35 PM
Hi,
I kwow STM32F4 support FSMC interface with LCD, FLASH...and SRAM/SDRAM...I have some example FSMC with LCD, SRAM but I don't kwow how to interface and control SDRAM. Can anyone show me an example (schematic, principles...) of STM32F4 FSMC interfacing with SDRAM?Thanks in advanced! #sdram #sdram-stm32f429-disco-expansion #stm32f4072015-04-24 6:08 AM
> Is it possible to attach that SDRAM to the FSMC
No (if you don't mind that I am not Clive). Read the fine manual, focus on FSMC vs. FMC. JW2015-04-28 8:29 AM
Jan,
thx a lot. I had not realised that from my mind... I have a SSD1963 connected to my STM32F407VGT6 in 16bit multiplexed mode. Now I wonder how to connect this external RAM in same mode to my uC: There are not so many fast SRAMS around... If someone had done that before and could give me some hints - fine ;o). Best, tom.2015-04-28 8:38 AM
You'll need to demultiplex the address lines for the SRAM, namely latch the lower addresses e.g. into a pair of 74HC573 or similar, driven by NADV. The rest of connections (NOE, NWE, higher address, data) are connected 1:1 between the mcu and memory.
You might want to start a new thread if you want to discuss this further. JW2015-10-18 8:53 PM
F407 only have FSMC, it cannot interface with SDRAM,
F42x have FMC, which can interface with SDRAMSee Reference Manual for F4xx, or data sheet for F4xx.Or you can use FSMC with a PSRAMWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.