cancel
Showing results for 
Search instead for 
Did you mean: 

tft lcd (LI48800T043TB3099Z02) interface with sdram (Winbond W9825G6KH) on stm32f479zit6

manoj89
Associate

i am try to interface tft lcd via LTDC using FMC, i checked that ram is working fine and test also passed , but i try to resolve lcd issue but it not resoled yes. Can someone help how to do that. i am uploading the complete project which is created. Please help how can i interface with lcd. 

2 REPLIES 2
Aimen1
ST Employee

Hello manoj89,

Please refer to the application note : Introduction to LCD-TFT display controller (LTDC) on STM32 MCUs - Application note, which provides a detailed description of the necessary steps to interface with the LCD.

Let me know if this helps you.

Regards.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

i worked on TFT, its working now , i am using stm32f476zit6 , ram , ltdc, on cubemx, but not able to rotate the display. i am attaching a picture. which show what i done. use another lcd having driver ic ICNL9701.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.