2013-02-14 4:47 AM
2013-02-14 5:21 AM
Don't be putting blocking functions like USART_puts(USART3, RBUF); in the interrupt?
2013-02-14 5:55 AM
Blocked function was deleted, I really have no need in it, because RBUF variable is a global variable, but the problem still here, chars doubling in random position of message.
Thank you for try. It goes worst: 1R0,Dm=004D,Dx=060D,Sn=0.0M,Sm=0.0M,Sx=0.1M,Taa=24.1C,Ua=31.5P,Pa=1007.1H,Rc=0.00M,Ri=0.0M,Hc=0.0M,HHi=0.0M,Th=24.0C,Vh=0.0N,Vs=12.0V,Vr=3.512V 1R0,Dm=348D,Dx=002D,Sn=0.0M,Sm=0.1M,Sx=0.1M,Ta=24.1C,Ua=31.5P,Pa=1007.1H,Rc=0.00MM,Ri=0.0M,Hc=0.0M,Hi=0.0M,Th=24.0C,Vh=0.0N,Vs=12.0V,Vr=3.510V 1R0,Dm=042D,Dx=066D,Sn=0.1M,Smm=0.1M,Sx=00.2M,Ta=24.2C,Ua=31.44P,Pa=1007.0H,Rcc=0.00M,Ri=0.0M,Hc=0.0M,Hi=0.0M,Th=24.0C,Vh=0.0N,Vs=12.0V,Vr=3.508V M,Sx=0.2M,Ta=24.2C,Ua=331.4P,Pa=1007.0H,Rc=0.00M,Ri=0.0M,Hc=0.0a=1007.0H,Rc=0.00M,Ri=0.0M,Hc=0.0M,Hi=0.0M,Th=23.8C,,Vh=0.0N,Vs=12.0V,Vr=3.510V .1M,Sx=00.2M,Ta=24.2C,Ua=31.44P,Pa=1007.0H,Rcc=0.00M,Ri=0.0M,Hc=0.0M,Hi=0.0M,Th=24.0C,Vh=0.0N,Vs=12.0V,Vr=3.508V 1R0,Dm=017D,Dx=017D,Sn=0.1M,Sm=0.1M,Sx=0.2M,Ta=24.2C,Ua=31.4P,Pa=1007.0H,Rc=0.00M,Ri=0.0M,Hc=0.0M,Hi=0.0M,Th=23.8C,,Vh=0.0N,Vs=12.0V,Vr=3.510V 1R0,Dm=032D,Dx=047D,Sn=0.0M,Sm=0.1M,Sx=0..1M,Ta=24.2C,Ua=31.4P,Pa=1007.0H,Rc=0.000M,Ri=0.0M,Hc=0.0M,Hi=0.00M,Th=23.8C,Vh=0.0N,Vs=12.0V,Vr=3.510V .1M,Sx=0.2M,Ta=24.2C,Ua=31.4P,P0.1M,Sx=0.1M,Ta=24.2C,Ua=31.4P,Pa=10077.0H,Rc=0.00M,Ri=0.0M,Hc=0.0M,Hi=0.0M,Th=24.0C,,Vh=0.0N,Vs=12.0V,Vr=3.510V 1M,Sx=0..1M,Ta=24.2C,Ua=31.4P,Pa=1007.0H,Rc=0.000M,Ri=0.0M,Hc=0.0M,Hi=0.00M,Th=23.8C,Vh=0.0N,Vs=12.0V,Vr=3.510V 1R0,Dm=062D,Dx=062D,Sn=0.0M,Sm=2013-02-14 9:17 AM
I don't have the time to wade into your project.
Of what I can see you really need to buffer and abstract the serial port data better. You need to be sending/receiving into some ring buffers of sufficient size, and have the interrupt shoveling the data as the USART is ready for it, at a singular point. Then you might want to look at data loss issues, whether you're losing stuff on the wire, or getting in to the buffer in multiple places, and if you need a mutex/semaphore to arbitrate access. The way you clear our RBUF is a complete waste of effort/resources.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.