2012-06-26 9:36 AM
Hi to all,
I started to develop a STM32F4-Discovery Soft Synth. A video showing it's first beta release is here:
http://www.youtube.com/watch?v=4JkhzH57Je4
In some post I view a interest to audio application using STM32F4-Discovery.
Can someone that have interest in audio processing give me some suggestion for the next release ? What kind of features to add ?2012-07-15 5:56 AM
Hi to all,
I got only some approval and some critical on my Soft Synth project. But I need some suggestion on how I must proceed in developing it ! Please, anyone have some suggestion on features to implement, or some possible application for it ? The project will be released as Open Source, so I want give a reusable version for many people. Best Regards, Alessandro.2012-07-16 1:35 AM
Your problem might by the targeted audience.
This forum is populated mostly by engineers, any deeper knowledge and interest in music is more or less coincidential. While I, for example, like to listen music sometimes, I have no intentions to make it myself... I rather suggest to post such a request to a forum dedicated to music. That probably results in a more purposeful feedback.2012-07-16 4:12 AM
Hello,
I'm a keyboard player and also a micro developer. Once, I had the idea to make a modular digital synthesizer (in order to have more voices) using STM32 micros. I'm talking about a real synthesizer for keyboard playing proposes, not a just a ''midi file player''. And that will be more nice to play: you could design your modular system (voice players, knobs, display, midi keyboard itnerface, computer interface) and so on! I think some type of ''WaveTable Synthesis'' will be more easy to develop Some youtube DIY synths: Keep the good work!2012-07-16 4:16 AM
Were is a forum I used to suft to discuss about DIY synth:
I think there are a lot of ideas there. And what about your synth? can you give more details about your implementation?2012-07-16 3:01 PM
Hello,
I'll look some ideas on your links. Thank you.However, the player you see is just an example. I would get something more than just an Midi-player :)
My synthesizer is developed keeping in mind the requirements for real-time. Each 'oscillator' processes a sample at a time, and makes it immediately available on the mixer outputs. All active 'oscillators' are processed in sequence so to obtain the output relative to a single mixed sample. In this stage, the latency is practically 0. Follows a post processing and writing in a small buffer used by the DMA for output. The buffer length determines in practice the latency from note-trigger to output.The suggestions that I ask are related to post-processing.
I not asked at musicians, because I already know what kind of answers I would get. Some engineers who knows both DSP and STM32F4 limits, can definitely give me some advice on some realistic algorithms to try. Alessandro2012-07-18 4:05 AM
What do you mean by ''post-processing'' ? Sound effects?
What type of synthesizer are you develop? there are lots of types of sound synthesisYou should make a block diagram of the synth you will implement. For ''effects'' I think that for STMF4 you cannot push it much, if you want speed and more voices.. so maybe you should choose fast and light algorithms. There is one good site: MRL2012-07-19 9:47 AM
Hi MRL,
I already known musicdsp.org from a long time and I use many of their contents.My project is a (improper defined) wavetable synth. It is a 'sample based' synth.
This tecnique was implemented after FM synthesis, first in some musical instrument and later in various PC sound cards. Each 'oscillator' consist in a interpolator chained with a envelope generator and a LP filter. There are other stage (modulators) to vary some parameter during note generation. There is also a global effect chain (pseudo reverber, chorus, graphic equalizer)STM32F4 is a powerful MCU but it do not have unlimited resource, so I will make the various features selectable at compiler time.
I will like to add some global post-process function as dinamic expander, antiliasing filter or any other low-computational DSP module.
But as FM said, this isn't a right place to ask similar questions, so I am sorry for this improper forum's utilization.
Best Regards to all again, Alessandro.
2012-07-19 11:38 AM
But as FM said, this isn't a right place to ask similar questions, so I am sorry for this improper forum's utilization.
You might have got this wrong. That's certainly not 'improper utilization', but you just have a quite low probability of getting really qualified feedback. Like finding the needle in the haystack.
2012-07-19 1:41 PM
Alessandro,
Your posting here is certainly welcome, it is fascinating to see the many and varied applications people have for the parts. fm's suggestion was more one of controlling expectations you might have about others participating here, and getting answers/feedback you want. While there are a small cadre of us that hang around here answering questions, for the most part forums like this are filled with people focused on their own, and often immediate, problems. -CliveWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.