2014-12-27 4:38 AM
I'm using Channel 1&3 in TIM1 to generate 4 Complementary PWMs (PA8, PA10, PB13, PB15, STM32F401VC DISCOVERY) to control my FullBridge DC-DC Converter.
In overcurrent or overvoltage cases, the PWM should be shutdowned to protect the MOSFETs. I'm using the following codes in Read_ADC() Procedure to do that.I wonder wheather these PWM Pin would be transfer to OpenDrain or connect to GND after shutdowned? And how could I connect GND for these Pins this case? This problem has influenced to the driver circuit and the MOSFETs very much.Can anyone help me?Thank you very much!!// Check Max_Cur and Max_Vb to disable PWM if ( Ir_Buf[Cur_Pos] > Max_Cur ) { TIM1->CR1 &= (uint16_t)(~TIM_CR1_CEN); TIM1->BDTR &= (uint16_t)~TIM_BDTR_MOE; TIM1->CCER &= (uint16_t)~(TIM_CCER_CC1E | TIM_CCER_CC1NE | TIM_CCER_CC3E | TIM_CCER_CC3NE); } if (Vb_Buf[Cur_Pos] > Max_Vb) { TIM1->CR1 &= (uint16_t)(~TIM_CR1_CEN); TIM1->BDTR &= (uint16_t)~TIM_BDTR_MOE; TIM1->CCER &= (uint16_t)~(TIM_CCER_CC1E | TIM_CCER_CC1NE | TIM_CCER_CC3E | TIM_CCER_CC3NE); }2015-12-28 10:16 PM
Can anyone help me? This problem can cause some incidents if I dont understand it in the root.
Thank you very much!!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.