2014-04-22 1:23 PM
Hi all,
does anybody have running gcc with simd for Cortex-M4 ? Kind regards,2014-04-24 4:45 AM
does anybody have running gcc with simd for Cortex-M4 ?
Can't say I've tried, but the hardware FPU stuff seems to work. Perhaps there are some more GNU/GCC centric forums or lists?2014-04-24 4:56 AM
does anybody have running gcc with simd for Cortex-M4 ?
I'm not aware that the M4 supports any SIMD instructions. The (optional) NEON unit on Cortex A devices does.
2014-04-24 7:41 AM
Hi
The programmers reference manual says that it does. https://my.st.com/sites/xnet_docs/drc/drc.aspx?documenttype=Programming%20Manual&prodtype=SS&prodid=1577&count=2 It only works on some Mult instructions. Not sure how much performance gain it is going to get!?!2014-04-24 8:39 AM
Have a look at core_cm4_simd.h in CMSIS directory of your toolchain.
[EDIT] Apparently gcc does use ''natively'' at least some of them, e.g. uint32_t aa(int32_t x, int32_t y) { int64_t acc; acc = x; acc += (int64_t) x * y; return (acc >> 32); } gcc 4.7.0 compiled into 0800019c <aa>: 800019c: 17c3 asrs r3, r0, #31 800019e: 4602 mov r2, r0 80001a0: fbc1 2300 smlal r2, r3, r1, r0 80001a4: 4618 mov r0, r3 80001a6: 4770 bx lr [EDIT2] Ah, smlal is not considered SIMD, sorry... :) JW2014-04-24 11:31 AM
Albeit even ARM talks about ''optimized SIMD ... instructions'', I view this as a rather overstretched definition of SIMD.
Just compare this with NEON or other MME/GPU unit, doing 32 ... 512 identical operations in parallel in a single instruction.2014-04-24 11:39 AM
fm ... please could you give me the hint ... is there processor in QFP package ?
2014-04-24 12:11 PM
Don't know, I'm no hardware designer. I would have to use a search engine, too.
NXP had produced LPC8xx Cortex-M0 MCUs in DIL package lately, so they might have QFP, too. Recently I am dealing with the x86 compatible embedded world, where everything is BGA...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.