2015-08-30 8:10 AM
Hello,
i see that if i activate the bootloader with BOOT0=1 and BOOT1=0 the system stay in the bootloader cycle all the time i mantain the pin configured in this way until restart the cpu. Is possible to jump directly to the main user program if after a timeout no request is coming from outside to the cpu?I'm asking because i have usually no access to the pcb when the final product is finished and i need to upload new program via bootloader. Thank you2015-08-30 8:37 AM
If you want to control the behaviour you need to get your own loader on the chip earlier in the process.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.