2014-03-13 1:34 PM
Can anyone tell me if the following is normal functionality of the RFR register:
Processor clock 168 MHz APB1 bus 42 MHz After reading the Receive FiFo and releasing by setting RFOM1 bit to 1 in the RF1R register, we must wait until the RFOM1 is reset to 0 by the hardware before exiting the interrupt. If we exit the interrupt while RFOM1 bit is still set, the interrupt routine is immediately re-entered and the subsequent reading of the RIR register returns a value with eroneous values. We never saw this issue using the an STM32F3 processor at 72 MHz and APB1 bus at 36 MHz. Thanks2014-03-13 1:42 PM
There are certainly race conditions with the NVIC, peripherals, and the tail-chaining mechanism with buses with significant disparity in speed.
It is important to clear interrupting sources early in the handler routines, and qualify the source upon entry. This isn't unique, a lot of people first encounter it with TIM interrupts. A read of the register prior to leaving the interrupt will force the pending write to complete, as will one of the memory fencing instructions.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.