STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with combining I/O devices on stm32f4discovery

Posted on March 12, 2014 at 13:20      Dear List, I have several problems with the use of multiple I/O devices at the same time. I have a number of stm32f4discovery boards to test. The software I use is build upon STM32_USB-Host-Device_Lib_V2.1.0, t...

Sietse by Associate III
  • 2072 Views
  • 9 replies
  • 0 kudos

STM32L05xx Initialization Files

Posted on March 11, 2014 at 22:09I am starting to bring up a board using an early engineering sample (ES32L053K8U6) very low power device, and would like to know if there already exists any library files, specifically:   system_stm32L0xx.s and / or ...

dcharla by Associate
  • 1116 Views
  • 2 replies
  • 0 kudos

One Pulse Mode with STM32F429DiscoveryBoard

Posted on March 13, 2014 at 11:45Hallo together,I want to use Timer 1 to capture a logic high input at Pin A9 and to create an output signal at Pin A10.I have written the following code which is derived from an STM32F10x example.I do not get any out...

CANopen Stack for STM32

Posted on March 14, 2014 at 08:40Hello,   I have seen two third Party  is supported a CANopen Stack for STM32 controller.  1. PRT 2. emtasI prefer emtas because i need EnergyBus frame. Before entering in to application, i want to know the memory foo...

SPI 9bit FOR STM32F0

Posted on March 14, 2014 at 07:25 Hello everyone. I'm working with STM32F0.I'm want to make 9 bits of data to be transferred via SPI. I've done the initial configuration for the SPI but it seems like the main program that I made wrong because...

sky_brake by Associate II
  • 1658 Views
  • 2 replies
  • 0 kudos

STM Flash Loder Demonstrator 2.6.0 & Win8 Bug

Posted on March 14, 2014 at 10:24Hi,there seems to be a bug with the flash loader GUI and win.8 / 8.1 and some MCU's bootloader.i have a STM32F050 here and when i try to connect to the bootloader with the flash loder tool it goes to the ''remove pro...

felix by Associate II
  • 1073 Views
  • 1 replies
  • 0 kudos

stm32f405 not running

Posted on March 14, 2014 at 00:33Dear all, i am trying some initial code on a stm32f405 that i could finally program. First thing i was wandering is if i can run (for test) straight with the internal HSI 16Mhz. Init code is from std stm32 library. ...

Angelo1 by Associate II
  • 896 Views
  • 1 replies
  • 0 kudos

STM32F4 bxCAN FiFo Release Issues

Posted on March 13, 2014 at 21:34Can anyone tell me if the following is normal functionality of the RFR register: Processor clock 168 MHz APB1 bus 42 MHz After reading the Receive FiFo and releasing by setting RFOM1 bit to 1 in the RF1R register, we...

STM32F0308-DISCOVERY RTC (32khz Osc)

Posted on March 13, 2014 at 16:59I am attempting to utilize the RTC on STM32F0308-Discovery board. I imported this code from the SMT32f standard peripheral library. However, while attempting to debug, the code hangs on command  /* Wait till LSE is r...

vendor by Associate II
  • 2004 Views
  • 2 replies
  • 0 kudos

stm32f405 minimal wiring

Posted on March 11, 2014 at 15:19Dear, i was trying to program stm32f405 through openpcd and a dcl5 parallel cable / interface that worked fine for other cortex cpu's. Until now i can't program successfully the device, so i am wandering what are the...

Angelo1 by Associate II
  • 1525 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.