2016-02-21 6:58 AM
Hello everyone,
I just started working on a personal project that includes image processing using a STM32f4 nucleo and an OV7725 camera.So by my calculations for a 9 fps rate and a 640x480 resolution,the camera outputs a 6 MHz pixel clock. It means that I have to read each byte from the parallel output port with a frequency of 6 MHz wich let me just 13-14 ticks (84/6) to save the byte and do other tasks.So this makes impossible acquisition.Could you guys give me an ideea how to manage this problem ? Thank you.2016-02-21 7:40 AM
This is where you use DCMI and DMA, but you'd still actually have to do something with the data. May be you need to think about just how much horse-power you need.
2016-02-21 9:13 AM
Thank you for your advice,I just read about the DCMI, I'm affraid stm32f4 series doesn't support DCMI tough,I checked the datasheet and there's nothing about DCMI.Maybe I just need to choose another board like stm32f2 (which supports DCMI) .
2016-02-21 9:31 AM
The one on the Nucleo might not, it's a 64-pin device.
Look at thehttp://www.st.com/web/en/resource/technical/document/reference_manual/DM00031020.pdf
for the STM32F4 devices, there is a whole chapter on DCMIThought of the Raspberry PI 2 running at 900 MHz, with 1GB of RAM? Something you might be able to do some video image capturing and processing with.2016-02-21 2:28 PM
Thank you very much,now it's clear for me.
Take care.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.