2015-06-22 7:15 AM
2015-06-22 8:05 AM
i need to read 2 adc channel simultaneously
Scanning really doesn't do that.If I needed 10 samples from TWO channels, I'd probably look to pair ADC1+ADC2, and use an advanced TIM that would do a 10x One-Shot (Repetition Count) A 5 MHz sample rate, and a 500 KHz interrupt rate, sounds like a fun project.2015-06-22 8:07 AM
2x 480 cycles for sample, wouldn't that be closer to 44 KHz than 5 MHz?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.