2015-06-21 10:19 PM
Hi
We are using STM32F205RCTbIs it possible to boot the controller from 0x08004000 location? if possible what are the places we need to modify the code. (Boot 0 and Boot 1 pins are already assigned to boot from Main flash)Please assist on this.2015-06-22 3:41 AM
Hello,
You can only boot from an offset 0 in your case is the 0x0800_0000 but you can execute a code from any address you want by specifying your memory Areas.I hope this answered your questions,Syrine.2015-06-22 4:33 AM
Hi
I am keeping my actual application code @ 0x0800C000 by changing ROM start area in IAR linker section, but keeping .intvecstart @0x08000000Will that suffice my requirement of executing code from 0x0800C000 location even after power on reset without any debuggerPlease correct me if my understanding is wrongThnaks2015-06-22 5:10 AM
Yes, as long as your vector table, or at least the two SP and PC entries, resides at 0x08000000, then the bulk of your code can be situated somewhere else.
You'd probably was to review the .MAP, and your created image to confirm things have been built in the manner you want/need.2015-06-22 7:42 AM
Hi Clive
Thanks for the clarification, it worked fine.However we are facing problem in firmware upgrade with Dfu utility, do we need to make any changes while creation of .dfu file or while downloading .dfu file, do we need to mention the address of init vector or address of code start(0x0800C000) anywhereRegardssangamesh2015-06-22 7:50 AM
I'd imagine if you feed the DFU Manager a working .HEX file, that would be sufficient.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.