2014-05-21 3:25 AM
I read the unique ID of STM32F407 microcontroller but i want to know what this unique ID represents means is there these bits can show any format or fields???
Is this ID represents the features of microcontroller if yes then how???2014-05-21 7:03 AM
The unique ID is only a number.
Out of all produced STM32 controllers it is one and only, therefore unique.2014-05-21 7:14 AM
There was supposedly some relation to the wafer id, and die location. ST uses the OTP ROM space to mark things like the RAM and/or FLASH size, and writing a bit vector to the AHB/APB peripheral clocks can also tell you what's available. ie CRYP/HASH
2014-06-18 8:38 AM
2014-06-18 9:55 AM
It's not a MAC ID either, they aren't random they are allocated. Burn your OWN number in OTP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.