2016-11-02 6:33 AM
where can found this definiton RCC_PLLSource_HSI
thanks for any help2016-11-02 7:30 AM
Hi,
RCC_PLLSource_HSI is defined understm32f30x_rcc.h#define RCC_PLLSource_HSI RCC_CFGR_PLLSRC_HSI_PREDIV /*!< Only applicable for STM32F303xE devices */
Regards
2016-11-02 8:04 AM
Please consider placing all related questions in a [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Compilation%20fails%20stdlib%20stm32f3x_rcc.c&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx¤tviews=15]single thread.
2016-11-02 8:25 AM
2016-11-02 8:41 AM
Suggests that you don't have the right defines passed to the compiler, and it is not including the files it needs properly.
With USE_STDPERIPH_DRIVER defined, you should just need to pull stm32f30x.h, and it in turn will pull stm32f30x_conf.h from your project directory, and the other includes it needs from the assorted peripheral files.2016-11-02 9:22 AM
I'm trying to compile the ST32F3Discovery project from ST using CrossStudio for Arm.
I have defined USE_STDPERIPH_DRIVER ant as target STM32F303VC. but more other defines are missed. for example RCC_CFGR_PLLNODIV , which is used in stm32F30x_rcc.c2016-11-02 9:52 AM
May be you can ''grep'' the files within the library to find these?
STM32F30x_DSP_StdPeriph_Lib_V1.2.3\Libraries\CMSIS\Device\ST\STM32F30x\Include\stm32f30x.h#define RCC_CFGR_PLLNODIV ((uint32_t)0x80000000) /*!< PLL is not divided to MCO */As I said, should be pulling stm32f30x.hMake sure that the compiler is searching the right Include file directories, in a suitable order.Try using an evaluation of a supported tool-chain, and review the template/example projects, then apply that to your chosen chain.Pay attention toa) Definesb) Project specific files and overall structurec) Include paths, to library copies, not tool-chain defaults2016-11-02 10:26 AM
i have compared the Crossworks stm32f30x.h with the file in the ST Library, they are different !!!
I have copied the file into the targets dir of Crossworks, now it works. ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.