2024-10-13 12:22 PM
Hi,
I run the NUCLEO-F303RE eval board. I separated the ST-Link part from the target processor part and connected GND/TCK/TMS/NRST/SWO by wires. I populated the 8MHz xtal with Rs and Cs on the target part.
This works fine.
I copied the circuitry for the target processor according to UM1724 documentation for my own board with populated xtal. I connected it to the ST-Link and flashed it with CubeIDE.
I read "Verifying ....." and "Download verified successfully" . So flashing seems to work.
Then I constantly get: "Target is not responding, retrying"
The xtal is not oscillating. The target processor does nort work either with direct MCO clock from ST-Link.
I checked Vdd and GND. I checked BOOT0 pin 10k to GND. VDDA and VBAT is not applied.
What does it need more to start?
THX Cheers
Detlef
Solved! Go to Solution.
2024-10-13 1:03 PM
VDDA/VSSA is required. It's not just if you use ADC/DAC, but it also runs the PLL and POR circuits.
2024-10-13 1:03 PM
VDDA/VSSA is required. It's not just if you use ADC/DAC, but it also runs the PLL and POR circuits.
2024-10-13 2:56 PM
:) . Yes, was not aware of that. Bought you a coffee or a beer.
Cheers
Thanks
Detlef
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.