STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Get the System Clock Frequency (SystemCoreClock)

Hi everyone,Help please,Im using CubeMX 5.0 with STM32F407 Disco board, I had activated the HSE clock to be the clock system with 168 MHz (HCLK on the clock tree of CubeMX).Im tryning then to get the CPU clock, ( to introduce it in the Basic systik m...

mmed by Associate III
  • 35568 Views
  • 6 replies
  • 3 kudos

Resolved! Odd observation on STM32G071 device

Hi allSTM32CubeIDE v1.16.1firmware package: cube FW_C0 V1.2.0I use the IDE to start a new project with STM32G071 on its discovery board.Just simply configure PD0, 1, 2, and 3 as inputs with pull-ups.  All other aspects are using IDE defaults.code gen...

STMG474 ADC Interleaved

Hi I am trying to get a high ADC sample rate "above 10MHz" with the STM32G4 family, I am playing with NucleoG474RE at the moment. I can see there is an example of Triple Multimode Interleaved for CubeF4 :STM32CubeF4/Projects/STM324x9I_EVAL/Examples/A...

Resolved! control of my stm32 with an external board

Good morning. I want to use my Nucleo to light up the LED of my stm32h747. For this, I first programmed a GPIO output for my nucleo board. I connected a wire and measured 3.4 volts and 120 mA with a multimeter. then, I decided to toggle the wire to p...

Capture d’écran 2024-10-13 à 15.48.09.png Jad_0-1728827361944.png
Jad by Senior
  • 2220 Views
  • 6 replies
  • 0 kudos

Resolved! The option bytes are not being written in STM32L433

I would like to enable write protection via an option byte.However, HAL_FLASH_OB_Launch() hangs, and even if the CPU is reset afterwards, the option byte is not rewritten.This issue occurs with both combinations: my board + J-Link or Nucleo + ST-Link...

Resolved! STM32F303 does not boot

Hi,I run the NUCLEO-F303RE eval board. I separated the ST-Link part from the target processor part and connected GND/TCK/TMS/NRST/SWO by wires. I populated the 8MHz xtal with Rs and Cs on the target part. This works fine.I copied the circuitry for th...

DetlefS by Senior
  • 1715 Views
  • 2 replies
  • 2 kudos

USB Package do not work

Hello,I have an Olimex board with an STM32F107 cpu on it.It start in the bootloader and I can upload firmware to it.For this I use CubeIDE and CubeProgrammer.I need to give USB support to my application so that to communicate with a PC.In CubeIDE, I ...

MDe by Associate III
  • 2978 Views
  • 4 replies
  • 0 kudos

problem w/ setting polynomial for CRC

I'm trying to set the polynomial for the CRC block and having some difficulty. I want to set the CRC block to compute a CRC-32K (Reversed Koopman) over my data.Here are the detailsCRC-32K (reversed Koopman polynomial) - 0xEB31D82EInput data - 0x31, 0...

wakeup STM32L0

HiMy name is Jonah and I’m working on STM32L031K4U6  .My device needs to go to standby, wake up via PA2(WKUP3) or RTC wakeupI follow  Doc RM0377 page 869 (to update PRER) , page 870(to update CR)If I write : RTC->CR          =0x00000404U;  ( WUTE=1 b...

yona by Associate
  • 1067 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.