cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303 Analog Comparator PINOUT

T B
Associate II

Hello!

I is allowed to use the same PIN for the COMP and the ADC?

I use the analog comparator as fast and software free PWM break input and I would like the measure the input with a ADC. I have tried it out and it was working. There was a small distortion from the sample and hold capacitor, but I can live with this.

Second Question:

Can I connect the DAC to the COMP only internally or do I need an PIN?

For Example I would like the use PA4 as ADC2_IN1 while DAC_OUT1 is used as

Input[-] for COMP1.

-Thomas

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.