2013-12-04 3:22 AM
Goodmorning,
I have a problem with the ADC calibration procedure: when I use stm32discovery kit, the software I made works. If I load the SAME SOFTWARE in the processor of application circuit, the calibration procedure never end. In both case the processor is STM32F303.NVIC_InitStructure.NVIC_IRQChannel = ADC1_2_IRQn; // canale di interrupt
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /*NVIC_InitStructure.NVIC_IRQChannel = ADC3_IRQn; // canale di interrupt NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);*/ //external_interrupt_config(); // SETTAGGIO CANALI ADC_DeInit(ADC1); ADC_DeInit(ADC2); ADC_DeInit(ADC3); ADC_DeInit(ADC4); /* Calibration procedure */ ADC_VoltageRegulatorCmd(ADC1, ENABLE); ADC_VoltageRegulatorCmd(ADC2, ENABLE); ADC_VoltageRegulatorCmd(ADC3, ENABLE); ADC_VoltageRegulatorCmd(ADC4, ENABLE); /* Insert delay equal to 10 µs */ Delay(10000); ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC1); ADC_SelectCalibrationMode(ADC2, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC2); ADC_SelectCalibrationMode(ADC3, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC3); ADC_SelectCalibrationMode(ADC4, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC4); while(ADC_GetCalibrationStatus(ADC1) != RESET ); calibration_value = ADC_GetCalibrationValue(ADC1);NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/*NVIC_InitStructure.NVIC_IRQChannel = ADC3_IRQn; // canale di interrupt
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);*/
//external_interrupt_config();
// SETTAGGIO CANALI
ADC_DeInit(ADC1);
ADC_DeInit(ADC2);
ADC_DeInit(ADC3);
ADC_DeInit(ADC4);
/* Calibration procedure */
ADC_VoltageRegulatorCmd(ADC1, ENABLE);
ADC_VoltageRegulatorCmd(ADC2, ENABLE);
ADC_VoltageRegulatorCmd(ADC3, ENABLE);
ADC_VoltageRegulatorCmd(ADC4, ENABLE);
/* Insert delay equal to 10 µs */
Delay(10000);
ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC1);
ADC_SelectCalibrationMode(ADC2, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC2);
ADC_SelectCalibrationMode(ADC3, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC3);
ADC_SelectCalibrationMode(ADC4, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC4);
while(ADC_GetCalibrationStatus(ADC1) != RESET );
calibration_value = ADC_GetCalibrationValue(ADC1);
The software never ends the while cycle.Vref+ and Vref- are quite the same in both circuits.Why the calibration procedure never ends? I don't think is a software problem. Is right to suppose is a hardware problem? Have you got any advice for explain the different behaviours?2013-12-04 8:07 AM
Not sure I understand some of the repetition of code here, but if it's hanging up in loops, you might want to pay particular attention to the clock sources, that they are enabled, and that the settings are valid.
2013-12-04 11:50 PM
/* Configure the ADC clock */
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2); /* Enable ADC1 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE); Yes, there's these instruction. The same code run correctly on the discovery kit but doesn't works on my application circuit. For this reason I suppose it's an hardware problem. I've attached the schematics. Is it correct? ________________ Attachments : Sheet1_Re520B.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0or&d=%2Fa%2F0X0000000be1%2FvDGq.5hqdbcwD0gfBrOjr4LRrh.fT6aW_jhvd.1ss8g&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.