2016-07-14 1:41 PM
I'm attempting a fairly standard initialization of the SPI peripheral on an STM32F302, and for some reason whenever I call GPIO_PinAFConfig(GPIOA, GPIO_Pin_15, GPIO_AF_6), the program jumps to the WWDG_IRQHandler. I've included a boiled-down version of the code which still reproduces this issue as well as a debug session demonstrating the problem below. Is there something obvious that I'm missing? The other AF configurations all work without any problem.
Source:
#include ''stm32f30x.h''
GPIO_InitTypeDef GPIO_InitStruct;
SPI_InitTypeDef SPI_InitStruct;
NVIC_InitTypeDef NVIC_InitStruct;
void
init(
void
);
void
main()
{
init();
for
(;;)
{
}
}
void
init()
{
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3, ENABLE);
// LED config
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
GPIO_Init(GPIOA, &GPIO_InitStruct);
// SPI config
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_15;
GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_PinAFConfig(GPIOB, GPIO_Pin_3, GPIO_AF_6);
GPIO_PinAFConfig(GPIOB, GPIO_Pin_4, GPIO_AF_6);
GPIO_PinAFConfig(GPIOB, GPIO_Pin_5, GPIO_AF_6);
GPIO_PinAFConfig(GPIOA, GPIO_Pin_15, GPIO_AF_6);
SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStruct.SPI_Mode = SPI_Mode_Slave;
SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;
SPI_InitStruct.SPI_NSS = SPI_NSS_Hard;
SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;
SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStruct.SPI_CRCPolynomial = 7;
SPI_Init(SPI3, &SPI_InitStruct);
SPI_RxFIFOThresholdConfig(SPI1, SPI_RxFIFOThreshold_QF);
SPI_Cmd(SPI3, ENABLE);
NVIC_InitStruct.NVIC_IRQChannel = SPI3_IRQn;
NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStruct.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStruct);
SPI_I2S_ITConfig(SPI3, SPI_I2S_IT_RXNE, ENABLE);
GPIO_SetBits(GPIOA, GPIO_Pin_0);
}
void
LED_On()
{
GPIO_ResetBits(GPIOA, GPIO_Pin_0);
}
void
SPI3_IRQHandler()
{
LED_On();
}
Debug session:
init () at src/main.c:43
43 GPIO_PinAFConfig(GPIOA, GPIO_Pin_15, GPIO_AF_6);
(gdb) s
GPIO_PinAFConfig (GPIOx=GPIOx@entry=0x48000000,
GPIO_PinSource=GPIO_PinSource@entry=32768,
GPIO_AF=GPIO_AF@entry=6 '\006')
at lib/STM32F30x_StdPeriph_Driver/src/stm32f30x_gpio.c:523
523 temp = ((uint32_t)(GPIO_AF) << ((uint32_t)((uint32_t)GPIO_PinSource & (uint32_t)0x07) * 4));
(gdb) s
514 {
(gdb) s
523 temp = ((uint32_t)(GPIO_AF) << ((uint32_t)((uint32_t)GPIO_PinSource & (uint32_t)0x07) * 4));
(gdb) s
524 GPIOx->AFR[GPIO_PinSource >> 0x03] &= ~((uint32_t)0xF << ((uint32_t)((uint32_t)GPIO_PinSource & (uint32_t)0x07) * 4));
(gdb) s
0x080006bc in WWDG_IRQHandler ()
2016-07-14 5:09 PM
Is there something obvious that I'm missing?
The most obvious thing would be the use of a GPIO_Pin_X mask instead of the GPIO_PinSourceX index.GPIO_PinAFConfig(GPIOA, GPIO_PinSource15, GPIO_AF_6);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.