2017-09-04 3:27 AM
Dear Sirs,
I have same problems to drive one SM-PMSM at ambient temperature of 65°C.At 25°C there is not any problem, all works as expected, but at 65°C a speed feedback error appear.
I checked the current sensing circuit, but all the electrical signals on the OPAMP, power supply are ok.
The ambient temperature close to the micro-controller (rated T85) is around 70°C.No any improvement if I change the motor BEMF parameter to compensate the BEMF changes due to the increased temperature.Here below my settings:
- STM32F301C8T6;- ST FOC library 4.2;- sensor-less (Observer+PLL);- one shunt and external OPAMP for the current sensing;- Torque control;- ambient temperature 65°C.Do you have some hints to find the cause of the problem?
Thank you in advance for the help
2017-09-04 9:56 AM
Dear L.G.,
speed feedback typically is caused by ripple in the speed estimation, in turn caused by worse current readings/response or misalignment of the motor model or speed PLL.
The easy: Try reducing G2 by factor two until the problem disappears. The same way you're however reducing probability of detecting stall.
The more difficult: look at DACs and compare what signals start deteriorating across the temperature. Good digital oscilloscope would help. Then, see which of the regulators may help tweaking.
2017-09-08 12:22 PM
Dear Edison,
the problem seems solved increasing the ADC clocks only.
But in this way the ripple of the estimated B-emf is increased a lot so I must increase the G2 in any case.
Thanks a lot, have a good day
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.