2015-05-11 11:35 PM
Hello
I'm using an STM32F302CB. I use this code to protect the first pages of code which contains a bootloader:[code]
uint32_t write_protected = FLASH_OB_GetWRP();uint32_t protect_mask = OB_WRP_AllPages - BOOTLOADER_WP;
/*
Bootloader
pages are not write protected.*/
if
(write_protected != protect_mask){
/*
* Unlock sequence
*/
FLASH_Unlock();
FLASH_OB_Unlock();
/*
* Enable WRP protection fails because factory default of the option flash is 00FF00FF00FFF.
* The function does a check for FFFF and an erase will set it to FFFF too.
* Therefore we do an erase of the option bytes before trying to protect the memory.
* This behavior is OK because no other settings of the option bytes excepts RDP is used.
*/
/*
* Clear flash flags
*/
FLASH_ClearFlag(FLASH_FLAG_EOP | FLASH_FLAG_WRPERR | FLASH_FLAG_PGERR | FLASH_FLAG_BSY);
if
(FLASH_OB_Erase() != FLASH_COMPLETE){
/*
* The best error handler we can do here is a reset
*/
NVIC_SystemReset();
}
/*
* Do some NOPs to take care of flash latency
*/
uint16_t loops = 40u;
while
(loops--){
__NOP();
}
/*
* Clear flash flags
*/
FLASH_ClearFlag(FLASH_FLAG_EOP | FLASH_FLAG_WRPERR | FLASH_FLAG_PGERR | FLASH_FLAG_BSY);
if
(FLASH_OB_EnableWRP(BOOTLOADER_WP) != FLASH_COMPLETE){
/*
* The best error handler we can do here is a reset
*/
NVIC_SystemReset();
}
/*
* Do some NOPs to take care of flash latency
*/
loops = 40u;
while
(loops--){
__NOP();
}
/*
* Write Protection OK, lock Flash and do
relaunch
of settings to ensure new settings are used.*/
FLASH_OB_Lock();
FLASH_Lock();
FLASH_OB_Launch();
}
[/code] IDE is IAR 7.4. Protecting the Flash pages is working. The Problem is I have some devices which have some Kind of locked Option Bytes. I tried JLinkSTM32.exe which is included in IAR to reset Option Bytes. I tried it manually via jlink. Nothing is working. I'm not able to Change Option Bytes anymore. RDP is _not_ set to 0xCC. It is set to 0xAA. Any idea what might be wrong? I have this issue with several Controllers. At the moment I have to unsolder the not working MCUs and replace them with working Versions. Thanks, Tilo2015-05-21 9:31 AM
Hi Tilo,
Did you tried to unlock the protection on your devices using the ST-Link Utility?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-06-08 10:56 PM
Hi
I have not used the ST utility yet because I only have the Segger J-Link JTAG. I will try to get the debugger.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.