2015-06-08 10:05 PM
Hi ,
I am using chan's FATFS with stm32f4 discovery,, So I could see that two paramateres, &sharpdefine _MAX_SS 512 and &sharpdefine BLOCK_SIZE 512 But when I change it to 4096 the FS is no longer able to open a File, Is the changing of these parameters advisable ? #stm32f4 #gpio #dma #discoveryWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.