2014-01-10 2:14 PM
I'm working with a STM32F373C8 and I'm trying to program flash while running a program on flash. This works well whenever I try to program the flash right at the beginning of my program. However, if I try to send a packet over USART after the initial startup, my program is stalling here:
FLASH_ErasePage(0x0800F800)
Does anyone know a reason why a program would stall here only after running for awhile? I'm unlocking the flash before, and locking it afterwards. Thanks for any help you can give to me.2014-01-13 3:08 AM
Hi
I am not familiar with the STM32F373C8 - so you will have to confirm by reading the data sheet. In general, you cannot write and read to the same Flash device while programming it ie you program is running in Flash and you are trying to program it! 2 solutions : 1 Program in a seperate program (often called a bootloader - not to be confused with the STM bootloader) 2 Move the SW download code into RAM2014-01-14 1:02 PM
Thanks for the response!
I thought that it is okay to program Flash while also running in flash, it just may incur delays. From several posts on this site as well as in the stm32f3 manual, I've heard that delays could range in the 40-50 ms range, but that would be alright for me. For my use case, a bootloader wouldn't work, but possibly loading into RAM could. I'll have to check that out.Anybody know why this ErasePage could be stalling for some other reason?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.