2015-01-26 5:48 AM
Hi,
It's already a few weeks I'm trying to bring up a solution of the USB Host via USB HS module with internal FS PHY. The same code works fine if I use OTG_FS module, once I pass to OTG_HS I'm starting to get a strange behavior which to my observation depends on some internal timing. I managed to get external device connection and exchanged a first SETUP read packet. But suddenly I found out that from time to time (about 10-20s not persistent) my OTG_HS host sporadically issues a RESET condition on the USB bus. I have seen 4ms drop on DP signal. After that I changed a bit an initialization sequence and got to the situation where OTG_HS can't properly detect device connection. It does detect but after some huge time of a 10-20min. GINTSTS also gives me a strange values that I can't explain. Below is the current initialization code. I do not use STM library but I went over library code and did exactly the same. (My initial version of the initialization works better but results in sporadic bus resets). This version has a detection problem so far./*
* IO & Clock Init
*/
if( REGS == USB_HS_REGS )
{
#ifdef CM5
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; /* Enable GPIOB Clock */
/* PB15 DM(D-), PB14 DP(D+) */
gpio_port_init( GPIOB, _IO(14)|_IO(15),
GPIO_MODE_ALT|GPIO_OUT_100M|GPIO_OUT_PP|GPIO_PULL_NO );
gpio_port_AF ( GPIOB, _IO(14)|_IO(15), AF_OTG_HS );
#endif
/* HS Module Clock Init */
RCC->AHB1ENR |= RCC_AHB1ENR_OTGHSEN;
}
else
{
#ifdef CM5
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN; /* Enable GPIOA Clock */
/* PA11 DM(D-), PA12 DP(D+) */
gpio_port_init( GPIOA, _IO(11)|_IO(12),
GPIO_MODE_ALT|GPIO_OUT_100M|GPIO_OUT_PP|GPIO_PULL_NO );
gpio_port_AF ( GPIOA, _IO(11)|_IO(12), AF_OTG_FS_HS );
#if 0
/* PA10 ID */
gpio_init( GPIOA,10,
GPIO_MODE_IN|GPIO_OUT_100M|GPIO_OUT_OD|GPIO_PULL_UP );
gpio_AF ( GPIOA,10, AF_OTG_FS_HS );
#endif
#endif
/* FS Module Clock Init */
RCC->AHB2ENR |= RCC_AHB2ENR_OTGFSEN;
}
RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN; /* Used for EXT INT Control */
/* Init Global AHB Configuration Register */
REGS->GREGS.GAHBCFG = 0; /* Disable USB Int */
REGS->GREGS.GUSBCFG |= GUSBCFG_PHYSEL; /* USB 1.1 Full-Speed */
/* Core SW Reset */
usb_core_sw_reset( REGS );
/* Deactivate Power down */
REGS->GREGS.GCCFG = GCCFG_PWRDWN|GCCFG_NOVBUSSENS;
vTaskDelay( 20/portTICK_RATE_MS );
/* Force Host mode */
REGS->GREGS.GUSBCFG |= GUSBCFG_FHMOD; /* Force Host Mode */
/*
* After setting the force bit, the application must wait at least 25 ms
* before the change takes effect.
*/
vTaskDelay( 50/portTICK_RATE_MS );
/* PHY Clock */
REGS->PCGCCTL=0; /* UnGate the PHY Clock */
vTaskDelay( 20/portTICK_RATE_MS );
/* Init Host Configuration Register */
REGS->HREGS.HCFG = HCFG_FSLSPCS_48; /* FS,CLK:48MHz */
usb_host_port_reset( REGS ); /* Reset port */
#if 0
REGS->HREGS.HPRT = HPRT_PPWR; /* Poweron Host port */
vTaskDelay( 50/portTICK_RATE_MS );
#endif
/*
* Configure IRQ
*/
REGS->GREGS.GINTMSK = 0; /* Mask all general INTs */
/* Configure NVIC */
if( REGS == USB_HS_REGS )
{
NVIC_SetPriority( OTG_HS_IRQn, IRQ_PRI_USB_HS );
NVIC_EnableIRQ( OTG_HS_IRQn );
}
else
{
NVIC_SetPriority( OTG_FS_IRQn, IRQ_PRI_USB_FS );
NVIC_EnableIRQ( OTG_FS_IRQn );
}
My code is waiting for Port Change IRQ but right now the GINTSTS = 0x14008
I do not understand why I get such a strange flags. USB device is connected to port.
Any help would be highly appreciated.
2015-03-07 12:44 AM
Any update?
2015-03-09 11:51 PM
Guys,
It's getting ridiculous. I'm not asking for special development or research, just to explain why things specified in data sheet are not working as expected and what to do to make them work.We are purchasing about 20K parts from ST annually and we expect to get some more dedicated treatment from ST support. Somehow we've lived so far with a luck of documentation and ''known'' bugs in ST core but this timeproblems mentioned above are showstopper for our development. Please take care to provide reply ASAP
.2015-03-10 1:23 AM
Hello Xol,
As you know, the forum isn't the official support channel for ST. The community is based on help exchange between members. Heisenberg has already taken into account your case, it may be under investigation.From my side also, I will go back to your questions and will keep you informed when I get more details on them.To increase its priority, it should be better to contact your FAE or local ST representative to describe more precisely your issue and wait for a deeper analysis. You may also submit a request on the/tmtrack/tmtrack.dll?ProjectPage&Template=submit&ProjectId=9&TableId=1011
.Best Regards,-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.