2014-07-14 6:38 AM
Hello
I’m using
https://kelectronics.eu/usvn/repos/EnvRegulator/trunk/Firmware/Env_Regulator/STM32F207VE.ld
and I have problems with RTC. I can configure it and write initialization data (time and date) and RTC seems to work ok. Time counter counts up every second but at 23:59:59 it
does not reset but still counts up (24:00:00, 24:00:01 … and so on!)
The second problem is when I write data using function:
RTC_SetDate(RTC_Format_BIN, &RTC_DateStructure)
And after checking RTC registers with JTAG I can see new data inside them. But every time when I call function RTC_GetDate(RTC_Format_BIN, &RTC_DateStructure) it returns old settings..:(
Only after reset RTC_GetDate(RTC_Format_BIN, &RTC_DateStructure) returns valid date, but when I set new date situation repeats….
Bellow my initialization code:/**
* @brief Configure the RTC peripheral by selecting the clock source.
* @param None
* @retval None
*/
void RTC_ConfigX(void)
{
#if (_USE_RTC_)
{
RTC_InitTypeDef RTC_InitStructure;
RTC_TimeTypeDef RTC_TimeStructure;
/* Enable the PWR clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);
/* Allow access to RTC */
PWR_BackupAccessCmd(ENABLE);
#if(RTC_CLOCK_SOURCE_LSI) /* LSI used as RTC source clock*/
/* The RTC Clock may varies due to LSI frequency dispersion. */
/* Enable the LSI OSC */
RCC_LSICmd(ENABLE);
/* Wait till LSI is ready */
while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET)
{
}
/* Select the RTC Clock Source */
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI);
SynchPrediv = 0xFF;
AsynchPrediv = 0x7F;
debug_printf(_LVL_5, ''RTC_Config LSI clock type setup\n'');
#elif(RTC_CLOCK_SOURCE_LSE) /* LSE used as RTC source clock */
/* Enable the LSE OSC */
RCC_LSEConfig(RCC_LSE_ON);
/* Wait till LSE is ready */
while (RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET)
{
}
/* Select the RTC Clock Source */
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);
SynchPrediv = 0xFF;
AsynchPrediv = 0x7F;
debug_printf(_LVL_5, ''RTC_Config LSE clock type setup\n'');
#else
#error Please select the RTC Clock source inside the main.c file
#endif /* RTC_CLOCK_SOURCE_LSI */
/* Enable the RTC Clock */
RCC_RTCCLKCmd(ENABLE);
/* Wait for RTC APB registers synchronisation */
RTC_WaitForSynchro();
/* Write to the first RTC Backup Data Register */
RTC_WriteBackupRegister(RTC_BKP_DR0, FIRST_DATA);
/* Set the Time */
RTC_TimeStructure.RTC_Hours = 0x00;
RTC_TimeStructure.RTC_Minutes = 0x00;
RTC_TimeStructure.RTC_Seconds = 0x00;
/* Set the Date */
/* Calendar Configuration */
RTC_InitStructure.RTC_AsynchPrediv = AsynchPrediv;
RTC_InitStructure.RTC_SynchPrediv = SynchPrediv;
RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24;
RTC_Init(&RTC_InitStructure);
/* Set Current Time and Date */
RTC_SetTime(RTC_Format_BIN, &RTC_TimeStructure);
RTC_SetCompilationDate();
/* Backup SRAM ***************************************************************/
/* Enable BKPRAM Clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_BKPSRAM, ENABLE);
/* Enable the Backup SRAM low power Regulator to retain it's content in VBAT mode */
PWR_BackupRegulatorCmd(ENABLE);
/* Wait until the Backup SRAM low power Regulator is ready */
while (PWR_GetFlagStatus(PWR_FLAG_BRR) == RESET)
{
}
/* RTC Backup Data Registers **************************************************/
/* Write to RTC Backup Data Register */
RTC_WriteBackupRegister(RTC_BKP0R, FIRST_DATA); //store first data to bacup reg
}
#endif
}
/**
* @brief Main RTC config function
* First it chcecks if rtc was configured and is maintain by external
* bacup voltage source
* If not RTC_ConfigX is executed
* @param None
* @retval None
*/
RTC_ConfigState_t RTC_Config(void)
{
RTC_ConfigState_t RTC_ConfigState;
#if(_USE_RTC_)
EXTI_InitTypeDef EXTI_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
//read first bacup register and check it has test data valid
if (RTC_ReadBackupRegister(RTC_BKP_DR0) != FIRST_DATA)
{
RTC_ConfigX();
debug_printf(_LVL_5,''RTC jeszcze nie konfigurowane\r\n'');
RTC_ConfigState=RTC_ConfigState_FirstConfig;
}
else
{
debug_printf(_LVL_5,''RTC już raz włącznone i skonfigurowane\r\n'');
RTC_ConfigState=RTC_ConfigState_NoNeedToconfig;
/* Enable the PWR clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);
/* Allow access to RTC */
PWR_BackupAccessCmd(ENABLE);
/* Wait for RTC APB registers synchronisation */
RTC_WaitForSynchro();
/* Clear the RTC Alarm Flag */
RTC_ClearFlag(RTC_FLAG_ALRAF);
/* Clear the EXTI Line 17 Pending bit (Connected internally to RTC Alarm) */
EXTI_ClearITPendingBit(EXTI_Line17);
/* Enable the PWR APB1 Clock Interface */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_BKPSRAM, ENABLE);
}
///-- Configure RTC Alarm A Interrupt
EXTI_ClearITPendingBit(EXTI_Line17 );
EXTI_InitStructure.EXTI_Line = EXTI_Line17;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
/* Enable the RTC Alarm Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = RTC_Alarm_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 4;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
#endif
return RTC_ConfigState;
}
/*******************************************************************************
*
* @fn RTC_SetCompilationDate
* @brief Set compilation date to RTC
* Author: kawel
* 06-06-2014
* @warning none
*
* @param void
*
* @return void
*
*******************************************************************************/
void RTC_SetCompilationDate(void)
{
uint8_t day, month, year;
int WeekDay;
RTC_DateTypeDef RTC_DateStructure;
debug_printf(_LVL_3, ''Compilation date: %s \r\n'', __DATE__);
if (RTC_GetDateFromCompilationDate(&day, &month, &year) == SUCCESS)
{
RTC_DateStructure.RTC_Date=day;
RTC_DateStructure.RTC_Month=month;
RTC_DateStructure.RTC_Year=year;
WeekDay=RTC_CalcDayOfWeek2(&RTC_DateStructure);
RTC_DateStructure.RTC_WeekDay=WeekDay;
RTC_SetDate(RTC_Format_BIN, &RTC_DateStructure);
}
}
#stm32f207ve-rtc-date-problem
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.