STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FSMC Base Address Calculation Problems

Posted on July 13, 2014 at 18:39Hello All, I have designed a board based on STM32F103VGT(100 pin, 1MB flash memory) which utilizes the FSMC to drive SSD1963 in 8 bit mode. I have connected FSMC_A17 to the SSD1963 RS, and FSMC_NE1 to SSD1963 CS. Afte...

STM32F407 Discovery

Posted on July 11, 2014 at 07:35Hi All,Can I program a STM32F401 mcu using STM32F407 Discovery board (STM32 ST-Link Utility is used for loading hex file).Currently I am getting a Unknown Device ID error Please let me know if any one had this issue b...

dibin by Associate II
  • 2281 Views
  • 4 replies
  • 0 kudos

RTC with HSE and STMF0

Posted on July 10, 2014 at 15:27I am trying to make a clock LCD display on my STM32F0. I want to use the external 8MHz crystal that is on my board. I cannot use any of the example code as none of it gives examples using the HSE. The code that I am u...

tracy by Associate II
  • 2823 Views
  • 6 replies
  • 0 kudos

GUI Library STM3241G EVAL BOARD PROBLEM

Posted on July 12, 2014 at 00:04Hi to all, I'm really new with STM products, I have a discover board STM3241G-EVAL, I'm going to try to explain my problem with the GUI embedded library: - The configuration of the source files is done, I can display ...

Change GPIO direction dynamically

Posted on July 10, 2014 at 14:39Hi AllI'm using an STM32L151 in my project.I have one GPIO configured as an input, and I need to change the direction dynamically. What is the most efficient way to do this ?Each time I want to change direction, shoul...

jerome2 by Associate II
  • 2051 Views
  • 2 replies
  • 0 kudos

STM32 SPI Problem receive only (with ADS1298)

Posted on December 30, 2012 at 16:16Dear all, I have just started working with STM32 microcontrollers (in this case it is a STM32F103VZE) coming from dsPIC controller family. I want to port a ECG system using the ADS1298 (from TI) from dsPIC to STM3...

gleich by Associate II
  • 5578 Views
  • 5 replies
  • 0 kudos

STM32F0- RS485 communication problem

Posted on July 09, 2014 at 12:39 Hi, I am trying to connect STM32F0 board with an energy meter. The Energy meter supports RS485 protocol. I have connected USART 2 to MAX 485 and the o/p of the MAX485 is connected to a level shifter 74ls25 an...

aruns06 by Associate II
  • 1990 Views
  • 4 replies
  • 0 kudos

jump from flash to RAM

Posted on July 13, 2014 at 14:19Hi,We have application that run in flash from address: 0x08000000.In order to update the application, we send loader code to the application through USB, the application copy the loader code in the RAM starting from a...

ilanh by Associate II
  • 1040 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.