2021-05-20 11:38 PM
#include<stdint.h>
#include "usart.h"
void
clock_init(void);
void
clock_init(void)
{
RCC->CR &= ~(RCC_CR_HSIDIV);
RCC->CR |= RCC_CR_HSION;
}
int
main()
{
clock_init();
usart_init();
while(1)
{
}
}
#include <stdint.h>
#include "stm32g0xx.h" // Device header
#include "usart.h"
void
isr(void);
uint8_t *ptr = "H";
uint8_t s = 2;
void
usart_init()
{
RCC->APBENR1 |= RCC_APBENR1_USART2EN;
GPIOA->AFR[0] |= GPIO_AFRL_AFSEL2_0;
GPIOA->MODER &= ~GPIO_MODER_MODE2;
GPIOA->MODER |= GPIO_MODER_MODE2_1;
GPIOA->AFR[0] |= GPIO_AFRL_AFSEL3_0;
GPIOA->MODER &= ~GPIO_MODER_MODE3;
GPIOA->MODER |= GPIO_MODER_MODE3_1;
NVIC_SetPriority(USART2_IRQn, 0);
NVIC_EnableIRQ(USART2_IRQn);
RCC->APBENR2 |= RCC_APBENR2_SYSCFGEN;
RCC->APBENR1 |= RCC_APBENR1_PWREN;
USART2->CR1 |= USART_CR1_TXEIE_TXFNFIE;
USART2->CR1 |= USART_CR1_TE;
USART2->BRR = 0x8B;
USART2->CR2 &= ~(USART_CR2_LINEN | USART_CR2_CLKEN);
USART2->CR3 &= ~(USART_CR3_SCEN | USART_CR3_HDSEL | USART_CR3_IREN);
USART2->CR1 |= USART_CR1_UE;
}
void
USART2_IRQHandler(void)
{
isr();
}
void
isr(void)
{
if (s == 0)
{
USART2->CR1 &= ~(USART_CR1_TXEIE_TXFNFIE);
}
else
{
USART2->TDR = (uint8_t)((*ptr) & (uint8_t)0xFF);
ptr++;
s--;
}
}
2021-05-21 1:04 AM
Read out and check the GPIO and UART registers content.
I don't see GPIO clock being enabled.
JW
2021-05-21 1:56 AM
I am sorry, the clock_init function actually had one more line. but while writing the question here, i did a mistake.
void clock_init(void)
{
RCC->CR &= ~(RCC_CR_HSIDIV);
RCC->CR |= RCC_CR_HSION;
RCC->IOPENR |= RCC_IOPENR_GPIOAEN;
}
I am enabling the clock of GPIOA too.
While running in debug mode, the TDR register also gets the 0x48 value(HEX code ASCII of character 'H').
still, on hercules application on my pc, i dont recieve anything.
using HAL USART driver, i could do it in 3 minutes, without any issue.
2021-05-24 12:42 PM
There are many small mistakes and many lines of unnecessary code, setting the bits which are already zeros to zeros.. The whole UART programming should take just 2 lines:
USART2->BRR = (HCLK_FREQ + BAUD_RATE / 2) / BAUD_RATE;
USART->CR1 = USART_CR1_RE | USART_CR1_TE | USART_CR1_UE.
No need to touch CR2 and CR3. No need to set IRQ priority to 0 - it s already 0 after reset. No need to enable HSI - it's already enabled.
Do not enable TXE interrupt untli you have something to send. Disable it BEFORE writing the last character to be sent.
If you can do it with HAL in 3 minutes, then without HAL it should take 1 minute, as you need 1/3rd of the code. ;)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.