2012-06-11 5:43 PM
I've recently created a prototype with a STM32F2 and a Solomon Systech SSD1963 interfaced via the FSMC (Resolution: 800 x 480). I've succeeded in getting things displayed on the screen, but I'm a little disappointed in performance. (Please note that I'm only referring to the amount of time it takes to write data to the SSD1963's frame buffer from the STM32F2, not the refresh rate of the LCD). I've only been able to get about 3 FPS and I was hoping for something in the teens.
Are my expectations too high? Please share your experience and offer your advice. Here's my FSMC init code. //--- FSMC Configuration ----------------------------------------------------- //FSMC Initialization FSMC_NORSRAMInitTypeDef FSMC_NORSRAMInitStructure; FSMC_NORSRAMTimingInitTypeDef FSMC_NORSRAMTimingInitStructure; // Enable the FSMC Clock RCC_AHB3PeriphClockCmd(RCC_AHB3Periph_FSMC, ENABLE); FSMC_NORSRAMDeInit(FSMC_Bank1_NORSRAM1); FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 0; // 1ns FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 1; // 2ns FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 1; // 4ns FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_B; //?? don't know yet FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 0; // Only used with NOR Flash FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 1; // Not used for Nor or SRAM FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0; // Don't care with Nor or SRAM FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1; FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_NOR; FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b; FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &FSMC_NORSRAMTimingInitStructure; FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &FSMC_NORSRAMTimingInitStructure; FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low; // Only valid for flash memory in burst mode (just default) FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState; // Only valid for burst memories (just default) FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable; // Only valid for flash memory in burst mode (just default) FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable; // Don't know yet FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable; // Don't know yet FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable; // Don't know yet FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; // Don't know yet FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable; // Don't know yet FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); // Enable FSMC Bank1_SRAM Bank FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM1, ENABLE); Thanks #ssd1963-lcd #lmgtfy #st32f2-fsmc #ssd1963-stm32f4-lcd-fsmc2012-06-11 11:50 PM
I guess your expectations are a little high.
This is 1/3 of a MByte of display RAM, considerably more than the available RAM of the controller. So you need to do all graphic operations in place, no double buffering. Generally, such a display belongs more to the 'Application' class - a task for the Cortex A devices, which have more RAM, performance and the appropriate hardware interfaces. I have a smaller display (32x240) with the same controller, driving it with GPIO. Its certainly good enough to bring information to the display - everthing called 'entertainment' becomes tricky with a Cortex M. You might need to add external RAM, and use DMA to do graphic operations.2012-06-12 5:40 PM
We have used 320x240 pixel data in 565 format.
Works ok on FSMC with DMA with refresh rate >30 Hz External RAM connected ofcourse.2012-06-12 11:37 PM
Hi all,
I'm also working on a project with a dumb TFT LCD (320 x 240). I'm trying to display static images (no double buffer). I've been able to display images (in 565 format) that I load on the flash memory using DMA and FSMC. I'm now trying to refresh the same images from external RAM using DMA again but I don't seem to get it right. What I'm doing is copying the images from the flash to the external memory using DMA and then refresh from the external memory.I thought maybe I wasn't writing to external RAM, I tried to view what's inside the external memory after writing and I was able to see the same data that is on flash.I based my approach on the AN3241.Can you guys please help me to see what I'm doing wrong.Thank you2012-06-13 12:09 AM
i can get around 25FPS with each pixel location (like paint dot with collor, paint another dot with another colour at new coordinate)
if i try to allocate ram and fill it with colour, i get 300FPS (so that would be for pictures, in theory i am geting 60FPS since that is panel limitation) i am using over-clocked STM32F4 at more than 200MHz core speed and ~60MHz gpio speedFSMC_NORSRAMInitTypeDef FSMC_NORSRAMInitStructure;
FSMC_NORSRAMTimingInitTypeDef FSMC_NORSRAMTimingInitStructure;
FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 1;
FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A;
FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1;
FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable;
FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_SRAM;
FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b;
FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;
FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;
FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;
FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable;
FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable;
FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;
FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;
FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);
FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 3;
FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 1;
FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0;
FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A;
FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;
FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);
FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM1, ENABLE);
and that is mine SSD1963 config with 8MHz PCLK (aka 60FPS for 480x272)
LCD_PinConfig();
LCD_FSMCConfig();
LCD_WriteCom(0x0001);Delay(500);
LCD_WriteCom(0x0011);Delay(500);
LCD_WriteCom(0x0029);Delay(500);
LCD_WriteCom(0x00E2);Delay(500);
LCD_WriteRAM(0x0021);Delay(500);
LCD_WriteRAM(0x0002);Delay(500);
LCD_WriteRAM(0x0004);Delay(500);
LCD_WriteCom(0x00E0);Delay(500);
LCD_WriteRAM(0x0001);Delay(500);
LCD_WriteCom(0x00E0);Delay(500);
LCD_WriteRAM(0x0003);Delay(500);
LCD_WriteCom(0x0001);Delay(500);
LCD_WriteCom(0x00E6);Delay(500);
LCD_WriteRAM(0x0002);Delay(500);
LCD_WriteRAM(0x0048);Delay(500);
LCD_WriteRAM(0x009E);Delay(500);
LCD_WriteCom(0x00B0);Delay(500);
LCD_WriteRAM(0x0028);Delay(500);
LCD_WriteRAM(0x0000);Delay(500);
//LCD Specification
LCD_WriteRAM((HDP>>8)&0X00FF);Delay(500);
LCD_WriteRAM(HDP&0X00FF);Delay(500);
LCD_WriteRAM((VDP>>8)&0X00FF);Delay(500);
LCD_WriteRAM(VDP&0X00FF);Delay(500);
LCD_WriteRAM(0x0000);Delay(500);
LCD_WriteCom(0x00B4);
LCD_WriteRAM((HT>>8)&0X00FF);
LCD_WriteRAM(HT&0X00FF);
LCD_WriteRAM((HPS>>8)&0X00FF);
LCD_WriteRAM(HPS&0X00FF);
LCD_WriteRAM(HPW);
LCD_WriteRAM((LPS>>8)&0X00FF);
LCD_WriteRAM(LPS&0X00FF);
LCD_WriteRAM(0x0000);
LCD_WriteCom(0x00B6);
LCD_WriteRAM((VT>>8)&0X00FF);
LCD_WriteRAM(VT&0X00FF);
LCD_WriteRAM((VPS>>8)&0X00FF);
LCD_WriteRAM(VPS&0X00FF);
LCD_WriteRAM(VPW);
LCD_WriteRAM((FPS>>8)&0X00FF);
LCD_WriteRAM(FPS&0X00FF);
LCD_WriteCom(0x00026);
LCD_WriteRAM(0x00002);
LCD_WriteCom(0x0035);
LCD_WriteRAM(0x0000);
// LCD_WriteCom(0x00BA);
// LCD_WriteRAM(0x000F); //GPIO[3:0] out 1
// LCD_WriteCom(0x00B8);
// LCD_WriteRAM(0x0007); //GPIO3=input, GPIO[2:0]=output
// LCD_WriteRAM(0x0001); //GPIO0 normal
// LCD_WriteCom(0x0036); //rotation
// LCD_WriteRAM(0x0000);
// LCD_WriteRAM(0x0060);
// LCD_WriteCom(0x0035); //rotation
// LCD_WriteRAM(0x0050);
// LCD_WriteCom(0x0026); //rotation
// LCD_WriteRAM(0x0003);
// LCD_WriteCom(0x0030); //rotation
// LCD_WriteRAM(0x0000);
LCD_WriteCom(0x00F0);
LCD_WriteRAM(0x0003);
LCD_Clear(BLACK);
LCD_WriteCom(0x0029); Also note that if you have configuration file from china (OPENMCU of something like that) they configurated driver for 10x slower operation for no good reasons, in my case that was around 5FPS refresh rate, now i have 8MHz pclk and 60FPS refresh rate.
try to overclock your F2 with PLL settings, and set that to maximum stable frequency
( but be careful, it will mess your timing critical applications)
2012-08-02 7:59 AM
Can I have your mail address because of direct contatct? I've got a small issule with DMA and SSD1963 together.
2013-03-26 10:33 AM
Hello, I am just trying something similar to what you've done. 7'' inch display (800 x 480) with SSD1963 and a STM32F4 Discovery board. Would you mind giving me the schematics of the interconnections between the LCD board and the STM board ? That would help me a lot, thanks.
Alberto2013-03-27 2:36 AM
7'' inch display (800 x 480) with SSD1963 and a STM32F4 Discovery board.
I hope you realize that is about 4 times the size of the internal RAM of the stm32f4, assuming 16 bit colors. Although it is feasible, you are limited in the capability to buffer graphics data, never mind drawing speed.
2013-03-27 4:13 AM
Yes, I know that. But the original poster succeeded in having an STM32F4 board driving the 7'' 800x480display, albeit at only 3 frames per second. For my application that is more than fast enough.
What I need is just the schematic of the electrical connections between the two boards.2013-03-27 7:19 AM
The SSD1963 has 1.2MB on board for a frame buffer, so the internal memory of the STM32F4 is of little import except for staging data from some external source like an SD Card.
It looks to use a pretty straight forward peripheral interfacing scheme. A number of people seem to have interfaced these to STM32, suggest you check via Google or eBay sellers of such.http://www.ebay.com/itm/7-Touch-Panel-SSD1963-TFT-LCD-Module-STM32-Dev-Board-/200641684729
http://www.egochina.net.cn/eBay/Download/AT070TN92_TP_SSD1963.pdf
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.