2018-06-23 2:22 PM
Hi
I want to parallel data transfer via DMA. I am trying to transfer an array in memory to the GPIO. For this, I thought it would trigger the DMA with the Timer Update event. In this way, I can move the data in memory to the GPIO.
In order to do this I have prepared the following init code.
void HUB75_Tim_DMA_Init(void)
{ __HAL_RCC_TIM3_CLK_ENABLE(); //Enable TIM3; __HAL_RCC_DMA1_CLK_ENABLE(); //Enable DMA1TIM_InitStruct.Instance = TIM3;
TIM_InitStruct.Init.Prescaler = 72-1; TIM_InitStruct.Init.CounterMode = TIM_COUNTERMODE_UP; TIM_InitStruct.Init.Period = 1000-1; TIM_InitStruct.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; TIM_InitStruct.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; TIM_InitStruct.Init.RepetitionCounter = 0; if (HAL_TIM_Base_Init(&TIM_InitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } DMA_InitStruct.Instance = DMA1_Channel2; DMA_InitStruct.Init.Direction = DMA_MEMORY_TO_PERIPH; DMA_InitStruct.Init.PeriphInc = DMA_PINC_DISABLE; DMA_InitStruct.Init.MemInc = DMA_MINC_ENABLE; DMA_InitStruct.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; // 16 bits DMA_InitStruct.Init.MemDataAlignment = DMA_PDATAALIGN_HALFWORD; DMA_InitStruct.Init.Mode = DMA_CIRCULAR; DMA_InitStruct.Init.Priority = DMA_PRIORITY_LOW; if (HAL_DMA_Init(&DMA_InitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } __HAL_LINKDMA(&TIM_InitStruct,hdma[TIM_DMA_ID_UPDATE],DMA_InitStruct); HAL_NVIC_SetPriority(DMA1_Channel2_IRQn, 0, 0); // enable DMA IRQ HAL_NVIC_EnableIRQ(DMA1_Channel2_IRQn); __HAL_TIM_ENABLE_DMA(&TIM_InitStruct, TIM_DMA_UPDATE); __HAL_TIM_ENABLE(&TIM_InitStruct); HAL_DMA_Start_IT(TIM_InitStruct.hdma[TIM_DMA_ID_UPDATE],(uint32_t)&my_buf, (uint32_t)&GPIOA->ODR, 100); }But this code did not work. There is no DMA interruption in any way. I must be making a mistake somewhere. Where?
Any idea? How can I do that?
#gpio #stm32 #timer #dma #data #parallel #transfer2018-06-23 3:22 PM
>> I must be making a mistake somewhere. Where?
TIM3_UP -> DMA1_CH3
2018-06-23 6:15 PM
that's we we use the cube, it separates the setup faults from the novice.
I couldn't work without the cube.
Like the Touch Sensing system.
what a nightmare,
and yet the hardware is really quite good.
I used the cube to setup the hardware but disabled the optional middleware.
Works like a treat, albeit convoluted
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.