2009-08-03 2:57 AM
STM32F10x Standard Peripherals Library v3.1.0
2011-05-17 4:19 AM
This version of the library defines the 'bool' type, FALSE and TRUE in the stm32f10x.h header on line 345.
The C-99 ANSI C standard defines 'bool' in the headerhttp://www.opengroup.org/onlinepubs/000095399/basedefs/stdbool.h.html
along with the values 'false' and 'true'. It also defines the symbol '__bool_true_false_are_defined'. This obviously results in a conflict if the end-user includes stdbool.h . Also the library doesn't appear to ever refer to 'bool', 'FALSE' or 'TRUE' anywhere. Therefore could ST please remove this from future versions of the library (it wasn't in v3.0.0) or at the least surround it by #ifndef __bool_true_false_are_defined #endifWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.