2012-07-13 1:37 AM
Hello
I have to use PB3 - PB4 - PB5 alternate function for using SPI3 or SPI1 But these pins are looking on JTAG main function after reset on datasheet.These pins are still working on jtag main function I can't change that.How can I solve this problem ?SPI Configuration is : void sFLASH_Init(void){ SPI_InitTypeDef SPI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; // &sharpifdef USE_STM3210C_EVAL//// /* Enable SPI3 Pins Software Remapping */// GPIO_PinRemapConfig(GPIO_Remap_SPI3, ENABLE);//&sharpendif /* Configure SPI_MASTER pins: SCK, MISO and MOSI */ GPIO_InitStructure.GPIO_Pin = sFLASH_SPI_SCK_PIN | sFLASH_SPI_MISO_PIN | sFLASH_SPI_MOSI_PIN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(sFLASH_SPI_GPIO_PORT, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = sFLASH_CS_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(sFLASH_CS_GPIO_PORT, &GPIO_InitStructure); /* 1 bit for pre-emption priority, 3 bits for subpriority */ NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4); /* Configure and enable SPI_MASTER interrupt -------------------------------*/ NVIC_InitStructure.NVIC_IRQChannel = SPI3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(sFLASH_SPI, &SPI_InitStructure); SPI_I2S_ITConfig(sFLASH_SPI, SPI_I2S_IT_TXE, ENABLE); /* Enable SPI_SLAVE RXNE interrupt */ SPI_I2S_ITConfig(sFLASH_SPI, SPI_I2S_IT_RXNE, ENABLE); SPI_Cmd(sFLASH_SPI, ENABLE); sFLASH_CS_HIGH();}RCC Configuration :void RCC_Configuration(void){ /* PCLK2 = HCLK/2 */ RCC_PCLK2Config(RCC_HCLK_Div2); /* Enable peripheral clocks --------------------------------------------------*/&sharpifdef USE_STM3210C_EVAL /* Enable GPIO clock for SPI_MASTER and SPI_SLAVE */ RCC_APB2PeriphClockCmd(sFLASH_SPI_GPIO_CLK | //SPI_SLAVE_GPIO_CLK | RCC_APB2Periph_AFIO, ENABLE); RCC_APB2PeriphClockCmd(sFLASH_CS_GPIO_CLK | RCC_APB2Periph_AFIO ,ENABLE); /* Enable SPI_MASTER Periph clock */ RCC_APB1PeriphClockCmd(sFLASH_SPI_CLK, ENABLE); &sharpendif}Pin Defines are : &sharpdefine sFLASH_SPI SPI3 &sharpdefine sFLASH_SPI_CLK RCC_APB1Periph_SPI3 &sharpdefine sFLASH_SPI_SCK_PIN GPIO_Pin_3 &sharpdefine sFLASH_SPI_MISO_PIN GPIO_Pin_4 &sharpdefine sFLASH_SPI_MOSI_PIN GPIO_Pin_5 &sharpdefine sFLASH_CS_PIN GPIO_Pin_1 &sharpdefine sFLASH_SPI_GPIO_PORT GPIOB &sharpdefine sFLASH_SPI_GPIO_CLK RCC_APB2Periph_GPIOB &sharpdefine sFLASH_CS_GPIO_PORT GPIOE &sharpdefine sFLASH_CS_GPIO_CLK RCC_APB2Periph_GPIOE #spi #jtag-pb4-remap #stm322016-01-14 8:49 PM
All, I read through this post in great detail as it almost completely describes the issue I am having. In my case I need PB3/PB4 for GPIO instead of SPI. All other PB bits work fine as GPIO and clearly PB3/4 are in JTAG mode. I'm using the 2-wire debug, so just trying to disable the dedicated JTAG pins. I've followed all the examples above and for some reason, no joy so guess I am missing something else fundamental.
1) making sure clocks go to GPIO blocks. 2) GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE); 3) Programming all 16 bits for GPIO_Mode_Out_PP I traced out the code in step two and it writes 0x0400_0000 to MAPR instead of 0x0200_0000 which is the value I'd expect from the datasheet. I tried writing 0x0200_0000 directly in case that was it, but no difference. I even tried disabling both debug ports with GPIO_PinRemapConfig(GPIO_Remap_SWJ_Disable, ENABLE), but can still hit the stop button in the IAR IDE and it stops things just fine, so seems as though I just can't disable JTAG. Any suggestions appreciated. New at this chip and tools, so figure I am missing something so obvious it isn't mentioned here. Thanks in advance. Using an STM32F100RB part if it helps. will2016-01-15 9:18 AM
Providing actual code usually beat trying to describe it.
I think this should adequately demonstrate,GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE); // GPIOB & AFIO
/* Configure PB.03 (JTDO) and PB.04 (JTRST) as output push-pull */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_4;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE); // Requires AFIO clock enabled, Map JTAG Off pins PB3,4 SWD still viable on PA13,14
while(1)
{
/* Toggle JTDO pin */
GPIO_WriteBit(GPIOB, GPIO_Pin_3, (BitAction)(1 - GPIO_ReadOutputDataBit(GPIOB, GPIO_Pin_3)));
/* Toggle JTRST pin */
GPIO_WriteBit(GPIOB, GPIO_Pin_4, (BitAction)(1 - GPIO_ReadOutputDataBit(GPIOB, GPIO_Pin_4)));
}
2016-01-15 9:34 AM
clive1:
OK, looking at your latest snippet, I think (hope) I see the issue. I am not enabling the RCC clocks to the AFIO block. That would be a nice and tidy explanation for everything I am seeing. Also good reminder to re-review clocks to every block in case I missed something else. Thank you, will post back after giving it a try this evening (US time). will2016-01-15 4:48 PM
Clive:
Yay! That was it. I missed that the AFIO functions had their own clock source independent from the rest of the GPIO. Thank you much for the help. willWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.