2016-06-10 4:29 AM
I'm trying to configure LIS3DH chip via SPI interface.
Here is my code:void init(void)
{
SPI_InitTypeDef SPI_InitStructure;
// SPI configuration
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; //4;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI_INT, &SPI_InitStructure);
// Enable SPI
SPI_Cmd(SPI_INT, ENABLE);
}
void set_up(void)
{
uint16_t buf = 0, msg = 0;
msg = READ + DEVICE_TYPE_REG;
//msg = 0x80 + 0x0F;
LIS3DHTR_CHIP_SELECT();
while (1) {
while (SPI_I2S_GetFlagStatus(SPI_INT, SPI_I2S_FLAG_BSY) == SET);
SPI_I2S_SendData(SPI_INT, msg);
while (SPI_I2S_GetFlagStatus(SPI_INT, SPI_I2S_FLAG_BSY) == SET);
if (SPI_I2S_GetFlagStatus(SPI_INT, SPI_I2S_FLAG_RXNE) == SET) {
buf = SPI_I2S_ReceiveData(SPI_INT);
if (buf == 51)
break;
}
}
LIS3DHTR_CHIP_DESELECT();
}
Problem: the lis3dh register with address 0x0F keeps constant 51 (type of device of something). When i send request to read this register (reg address plus set MSB bit) via spi interface stm32f107 spi RX register gives me 0xFF at first. And only on second iteration of cycle (while(1)) i get true This problem appears on every my request to lis3dh chip.
Is it normal or have i missed something?
#stm32f107 #lis3dh #mems
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.