2020-03-05 1:02 AM
I am configure w5100 using spi.but at the time of reading its show wrong data.
Refer Code link: https://www.carminenoviello.com/2015/08/28/adding-ethernet-connectivity-stm32-nucleo/
2020-03-05 3:28 AM
have you done right pin configuration
2020-03-05 3:30 AM
if your pin configuration is right then delay could be the reason
2020-03-05 8:14 PM
GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);
GPIO_InitStructure.GPIO_Pin=ETH_SCK | ETH_MOSI | ETH_MISO ;
GPIO_InitStructure.GPIO_Mode=GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed=GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin=ETH_SS;
GPIO_InitStructure.GPIO_Mode=GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed=GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
2020-03-05 8:19 PM
yes but at the starting time for setting and getting ip return from w5100 showing wrong data.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.