2019-11-03 1:00 AM
hello. I have a question using uart(115200, 8, 0,1) in stm32f103vct6.
huart3->gstate have been changed hal_busy forever In an unspecified situation and system is halted.
I use true studio compiler. and In debug mode at that time, systick interrupt is running but main loop is not working.
I use hal_uart_transmit_it and hal_uart_receive_it. I think it's not problem that uart3 buffer overflow.
and the value of uart3 sr register is 0xf8.(Overrun error)
i wanna clear this issue as soon as possible.
what should I check and how can I clear this issue??
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.