2016-11-04 8:48 AM
While debugging an issue I discovered that on the STM32F103RD/VD silicon, GPIOC pin 2 defaults to SET/1 in the ODR. All other GPIO ports default to RESET/0. While it is always good practice to explicitly set the ODR to a default state, in our case we were simply changing GPIOC_2 to a push-pull output and got quite a surprise when the connected circuit went active.
I didn't see this listed in the ST errata document for the STM32 high-density line (DocID14732 Rev 14 / ES0340). Thought this might help others experiencing unexpected behavior on GPIOC.2016-11-04 2:04 PM
I've used STM32 parts for the last 9 years, and not seen this, so I'm rather skeptical. Are you sure it's not a board, debugger, or configuration issue?
2016-11-06 10:36 AM
How exactly do you test it (with issues Clive listed above in mind)?
Is this on one particular piece, or can you reproduce it on a different one/different batch (datecode)? JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.