2017-02-28 4:17 PM
Hello,
I'am using and STM32F103C8T6 development board to communicate via SPI with ADS1220(Analog to Digital Converter). My code needs to read the buffer of the ADS1220 at certain times. When i run the code the SPI works only for a few minutes(max 14 min) before it stops. The SPI code i am using is :
void SPIx_Init()
{
// Initialization struct SPI_InitTypeDef SPI_InitStruct; GPIO_InitTypeDef GPIO_InitStruct;// Step 1: Initialize SPI
RCC_APB2PeriphClockCmd(SPIx_RCC, ENABLE); SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; SPI_InitStruct.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b; SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStruct.SPI_Mode = SPI_Mode_Master; //SPI_InitStruct.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set; SPI_Init(SPIx, &SPI_InitStruct); SPI_Cmd(SPIx, ENABLE); // Enables SPIx peripheral.// Step 2: Initialize GPIO
RCC_APB2PeriphClockCmd(SPI_GPIO_RCC, ENABLE);// GPIO pins for MOSI and SCK
GPIO_InitStruct.GPIO_Pin = SPI_PIN_MOSI | SPI_PIN_SCK; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz; GPIO_Init(SPI_GPIO, &GPIO_InitStruct);// GPIO pins for MOSI, MISO
GPIO_InitStruct.GPIO_Pin = SPI_PIN_MISO; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz; GPIO_Init(SPI_GPIO, &GPIO_InitStruct);}
uint8_t SPIx_Receive(uint8_t data)
{ // Write data to be transmitted to the SPI data register SPIx->DR = data; // Wait until transmit complete while (!(SPIx->SR & (SPI_I2S_FLAG_TXE))); // Wait until receive complete while (!(SPIx->SR & (SPI_I2S_FLAG_RXNE))); // Wait until SPI is not busy anymore while (SPIx->SR & (SPI_I2S_FLAG_BSY)); //Return received data from SPI data registerreturn SPIx->DR;
}
The program always stops at this line of code :
while (!(SPIx->SR & (SPI_I2S_FLAG_TXE)));
Before the code stops, it has done at least 1000 reads(usually more than a 1000,maybe even 50000) of the buffer successfully. Why does my code stop after successfully running for so long time. Is there a problem with the SPI buffer, some data not being send. The data I am transmitting is a dummy byte 0x00.
Any help would be greatly appreciated.
2017-03-01 2:27 AM
//SPI_InitStruct.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set;
So NSS is undefined, then?
JW
2017-03-01 5:55 AM
I mean, you MUST initialize it somehow in the SPI_InitStruct, otherwise - as it's a local variable - it's sort of random what will it be set to.
And, if the pin is not used, use Soft and set it to low.
JW
2017-03-01 6:46 AM
Yes, i don't need it. The chip select of the ADS1220 is tied low. I am only communicating with one slave on the SPI.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.