2017-05-02 3:06 AM
Dear All,
I have some problems with receiving DMX-512 data on a STM32F103RB.
I am using mbed and the library i found for this is meant for the F303 version.
When i look at the Typedef _uart there is a difference in those 2 chips in the uart registers.
void
DMX::int_rx () {int
flg, dat;#ifdef TARGET_STM
dat = _dmx.getc
(); flg = (_uart->ISR & (USART_FLAG_FE | USART_ISR_IDLE)) == (USART_FLAG_FE | USART_ISR_IDLE);if
(flg) { _uart->ICR = USART_ICR_FECF; }Since ISR and ICR are not in that typedef i get errors on the flag, but i don't know how i can fix this.
Could anyone help me with this?
Thank you in advance!
2017-05-02 5:00 AM
What is your DMX software based on, in regard to STM ?
In the SPL for the F30x, those registers still exist. A snippet from stm32f30x.h:
typedef struct
{
__IO uint32_t CR1; /*!< USART Control register 1, Address offset: 0x00 */
__IO uint32_t CR2; /*!< USART Control register 2, Address offset: 0x04 */
__IO uint32_t CR3; /*!< USART Control register 3, Address offset: 0x08 */
__IO uint16_t BRR; /*!< USART Baud rate register, Address offset: 0x0C */
...
__IO uint32_t
ISR
; /*!< USART Interrupt and status register, Address offset: 0x1C */__IO uint32_t
ICR
; /*!< USART Interrupt flag Clear register, Address offset: 0x20 */__IO uint16_t RDR; /*!< USART Receive Data register, Address offset: 0x24 */
uint16_t RESERVED4; /*!< Reserved, 0x26 */
__IO uint16_t TDR; /*!< USART Transmit Data register, Address offset: 0x28 */
uint16_t RESERVED5; /*!< Reserved, 0x2A */
} USART_TypeDef;
And, instances are declared in capital letters in the same file:
#define USART2 ((USART_TypeDef *) USART2_BASE)
#define USART3 ((USART_TypeDef *) USART3_BASE)
#define UART4 ((USART_TypeDef *) UART4_BASE)
#define UART5 ((USART_TypeDef *) UART5_BASE)
...
Seems you need to re-write some parts ...
2017-05-02 5:51 AM
Yes I know they are available for the STM32F30x stuff, but I am using the STM32F103.
So in that SPL they are not available, but what can i use for those registers?
2017-05-02 8:40 AM
Ahh, got the porting direction wrong.
The F10x has a different register interface (to the USART peripheral and other peripherals):
typedef struct
{
__IO uint16_t SR;
uint16_t RESERVED0;
__IO uint16_t DR;
uint16_t RESERVED1;
__IO uint16_t BRR;
uint16_t RESERVED2;
__IO uint16_t CR1;
uint16_t RESERVED3;
__IO uint16_t CR2;
uint16_t RESERVED4;
__IO uint16_t CR3;
uint16_t RESERVED5;
__IO uint16_t GTPR;
uint16_t RESERVED6;
} USART_TypeDef;
That probably means a re-write of several sections. Not sure about mbed and available libraries, I never used it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.