2016-04-05 3:57 AM
Hi,
I am trying to build a slave using a STM32F103. I've got the ''Optimized I2C Examples'' project to use it as a base and I get the idea of what is happening.The bit I am stuck at is finding a way to check if master is trying to read or write. I cannot seem to find any info in the reference manual.In my I2C2_EV_IRQHandler I've implemented the I2C_EVENT_SLAVE_RECEIVER_ADDRESS_MATCHED and I can see it being matched if I try to read or write from master, but cannot find a way to let slave identify what master wants.(The my.st forum won't let me add code properly as the site seems to have an error)void I2C2_EV_IRQHandler(void){ __IO uint32_t SR1Register =0; __IO uint32_t SR2Register =0; /* Read the I2C2 SR1 and SR2 status registers */ SR1Register = I2C2->SR1; SR2Register = I2C2->SR2; /* If I2C2 is slave (MSL flag = 0) */ if (I2C_GetFlagStatus(I2C2,I2C_FLAG_MSL) == RESET) { /* If ADDR = 1: EV1 */ if (I2C_CheckEvent(I2C2,I2C_EVENT_SLAVE_RECEIVER_ADDRESS_MATCHED)) { regVal = I2C_ReadRegister(I2C2,I2C_Register_OAR1); /* Clear SR1Register SR2Register variables to prepare for next IT*/ SR1Register = 0; SR2Register = 0; /* Initialize the transmit/receive counters for next transmission/reception using Interrupt */ Tx_Idx2 = 0; Rx_Idx2 = 0; fs = I2C_GetFlagStatus(I2C2,I2C_FLAG_TRA); } /* If TXE = 1: EV3 */ if ((SR1Register & 0x0080) == 0x0080) { /* Write data in data register */ I2C2->DR = Buffer_Tx2[Tx_Idx2++]; SR1Register = 0; SR2Register = 0; } /* If RXNE = 1: EV2 */ if (I2C_CheckEvent(I2C2,I2C_EVENT_SLAVE_BYTE_RECEIVED)) { /* Read data from data register */ Buffer_Rx2[Rx_Idx2++] = I2C2->DR; SR1Register = 0; SR2Register = 0; } /* If STOPF =1: EV4 (Slave has detected a STOP condition on the bus */ if (( SR1Register & 0x0010) == 0x0010) { I2C2->CR1 |= CR1_PE_Set; SR1Register = 0; SR2Register = 0; } } /* End slave mode */ /* If SB = 1, I2C1 master sent a START on the bus: EV5) */ if ((SR1Register &0x0001) == 0x0001) { /* Send the slave address for transmssion or for reception (according to the configured value in the write master write routine */ I2C1->DR = Address; SR1Register = 0; SR2Register = 0; } } #i2c-slave-stm32f1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.