2014-05-10 8:58 AM
Hello
I am searching for the way how to protect my chip. It should:- protect flash memory from reading in all cases, even if somebody flashes his own firmware.- allow to upload new firmware with stock bootloader (usart) - only XX pages are erased/replaced.- allow to read/write flash only from my firmware.I need to protect especially one flash page, other pages are irelevant.Do you think it is even possible with RDP or different technique?Thank you very much #flash-protection2014-05-10 9:10 AM
- protect flash memory from reading in all cases, even if somebody flashes his own firmware.
How would that work? Even with RDP the code running in flash can read the entire memory space. You can't get the level of partitioning you seek.2014-05-10 3:21 PM
Well, that is unclear to me too but I know it could be used as attack.
Simply I need to protect one page of memory from reading. It should be accessible only from my (trusted) firmware.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.