2017-09-10 9:00 AM
I try to configure my MCO ouput on my STM32f103, only with STD periph lib.
here is my code:
void OutputMCO() { GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /* Output clock on MCO pin ---------------------------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); // pick one of the clocks to spew //RCC_MCOConfig(RCC_MCOSource_SYSCLK); // Put on MCO pin the: System clock selected //RCC_MCOConfig(RCC_MCOSource_HSE); // Put on MCO pin the: freq. of external crystal //RCC_MCOConfig(RCC_MCOSource_PLLCLK_Div2); // Put on MCO pin the: System clock selected }
I have an issue here:
// pick one of the clocks to spew //RCC_MCOConfig(RCC_MCOSource_SYSCLK); // Put on MCO pin the: System clock selected //RCC_MCOConfig(RCC_MCOSource_HSE); // Put on MCO pin the: freq. of external crystal //RCC_MCOConfig(RCC_MCOSource_PLLCLK_Div2); // Put on MCO pin the: System clock selected
None of the 3 possibilities are working on my code. This code was found on internet. Do you know where should I find correct parameters ? The definition of RCC_MCOSource doesn't really help me
Thank you
#stm32f103 #mco #stm32-mco-clock-outputSolved! Go to Solution.
2017-09-10 11:41 AM
STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\RCC\RCC_ClockConfig\main.c
/* Output HSE clock on MCO pin ---------------------------------------------*/
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); RCC_MCOConfig(RCC_MCO_HSE);2017-09-10 11:41 AM
STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\RCC\RCC_ClockConfig\main.c
/* Output HSE clock on MCO pin ---------------------------------------------*/
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); RCC_MCOConfig(RCC_MCO_HSE);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.